Our Company
Company Profile
Awards and Recognition
Our Values
Featured Stories
2013 Edison Award
Automotive Innovations Award 2013
Chery Jaguar Land Rover
Supporting Wounded Warriors
Auto Shanghai 2013
2013 Best Corporate Citizens
Diverse IT Professionals
Electronic Cockpit
2012 Kepner-Tregoe Award
Diverse engineers
Bespoke Interior
Garbsen playground
Ethisphere 2013
Hip-point mannequin
Junior Achievement
Better Buildings Challenge
Red Lion High School
Inspiration Seat
Governor's Ambassador Award
Sustainable Energy Factbook
Improving pediatric medicine
Hongqi H7
Ford Fusion Auto Start-Stop
Compression Hybrid Molding
Micro Hybrid Battery
2013 CES
Sound & Vibration Lab
Top Employer in China 2013
Green Masters Program
Executive Involvement & Steering Program
Investor relations honors
Joint Center for Energy Storage Research
Holland battery plant
Journey from the heart
Red Cross Disaster Relief
Instituto Nacional de Cancerología
Blue Sky Involve
ÖkoGlobe 2012
Corporation of the Year
Sustainability in the schools
Electric vehicle donation
Florence recycling facility
World Medical Relief
Innovative training
Safety first at Oak Ridge
Understanding Digital Natives
Chillers in mines
End-user research
Recycled resin
Green jobs for youths
AGM battery technology
Puerto Rico train stations
2012 Energy Efficiency Forum
Automotive Interiors Awards
Hospital for Sick Children
World Environment Day
Start-Stop research
Best Corporate Citizens List
Our Businesses Our Leaders Our People Our Diversity Our Community Focus Our Corporate Governance Our History Social Media
mannequin_466

Johnson Controls has developed a process for calibrating its hip-point measuring mannequins that ensures an especially high degree of accuracy and precise reproducibility of the process.

Johnson Controls develops new hip-point mannequin that complies with international standards

Hip-point mannequins are an indispensible element in the engineering and production of automotive seating, used to measure whether a vehicle can safely and comfortably accommodate the driver and passengers. Since there are three different international standards that define the characteristics and dimensions of these mannequins, automakers and suppliers use various models.

 

Johnson Controls, the world’s leading manufacturer of automotive seating, recently developed a hip-point mannequin that complies with all three standards.

 

“As a technology leader in automotive seating, we measure and test our products every day in order to ensure the greatest possible safety and optimal comfort,” said Dr. Wilfried Beneker, vice president engineering, product business unit metals and mechanisms at Johnson Controls Automotive Seating. “Until now, however, there was no single hip-point mannequin on the market that satisfied all three standards and our high requirements. Therefore, it made sense for our engineers to design their own mannequin.”

 

The new hip-point mannequin from Johnson Controls meets standards set by the Society of Automotive Engineers (standard SAE J 826), the central specification for hip-point mannequins worldwide, and the GLORIA standard for EuroNCAP tests. It also satisfies recommendations of the German Association of the Automotive Industry VDA (recommendation VDA 304).

 

The hip point plays a key role in the development of automotive seating. It is the seating reference point (SgRP) in digital design plans. Measurements are defined from this point in the vehicle, including the distance to the steering wheel and gas pedal and the driver’s field of vision. Using a hip-point mannequin, the position of the driver and passengers can be measured in prototypes and as well as in the actual vehicle and then compared with the design plans.

 

mannequin_226

The measuring mannequin from Johnson Controls, with its carbon torso, can also be fitted with a head restraint measurement device (HRMD). This determines the position of the head in relation to the head restraints.

 

Engineers at Johnson Controls have also developed a procedure for calibrating the hip-point mannequin and head restraint measurement device. The mannequin is clamped into a calibration device and measured with a 3D coordinate measuring machine. An optical 3D scanning system is used to test that the carbon torso shell fully meets all standards after production as well.

 

This method ensures an especially high degree of measurement accuracy and precise reproducibility of the process. In addition, the engineers have also defined a detailed but user-friendly calibration log. This allows users of the mannequin and head restraint measurement device to easily check adherence to the detailed specifications contained in the three standards.

Johnson Controls has been using the hip-point mannequin since June 2011. Following in-house practical testing for a year and a half, the company is now offering the mannequin to automakers, other manufacturers of automotive seating and external testing organizations.

 

“The response to our mannequin has been extremely positive. Several automakers have already shown interest in it,” said Dr. Beneker.