Our Company
Our Businesses
Our Leaders
Our People
Our Diversity
Our Community Focus
Our Corporate Governance
Our History
Social Media
| ► | Company Profile |
| ► | Awards and Recognition |
| ► | Our Values |
| ▼ | Featured Stories |
| • | 2013 Edison Award |
| • | Automotive Innovations Award 2013 |
| • | Chery Jaguar Land Rover |
| • | Supporting Wounded Warriors |
| • | Auto Shanghai 2013 |
| • | 2013 Best Corporate Citizens |
| • | Diverse IT Professionals |
| • | Electronic Cockpit |
| • | 2012 Kepner-Tregoe Award |
| • | Diverse engineers |
| • | Bespoke Interior |
| • | Garbsen playground |
| • | Ethisphere 2013 |
| • | Hip-point mannequin |
| • | Junior Achievement |
| • | Better Buildings Challenge |
| • | Red Lion High School |
| • | Inspiration Seat |
| • | Governor's Ambassador Award |
| • | Sustainable Energy Factbook |
| • | Improving pediatric medicine |
| • | Hongqi H7 |
| • | Ford Fusion Auto Start-Stop |
| • | Compression Hybrid Molding |
| • | Micro Hybrid Battery |
| • | 2013 CES |
| • | Sound & Vibration Lab |
| • | Top Employer in China 2013 |
| • | Green Masters Program |
| • | Executive Involvement & Steering Program |
| • | Investor relations honors |
| • | Joint Center for Energy Storage Research |
| • | Holland battery plant |
| • | Journey from the heart |
| • | Red Cross Disaster Relief |
| • | Instituto Nacional de Cancerología |
| • | Blue Sky Involve |
| • | ÖkoGlobe 2012 |
| • | Corporation of the Year |
| • | Sustainability in the schools |
| • | Electric vehicle donation |
| • | Florence recycling facility |
| • | World Medical Relief |
| • | Innovative training |
| • | Safety first at Oak Ridge |
| • | Understanding Digital Natives |
| • | Chillers in mines |
| • | End-user research |
| • | Recycled resin |
| • | Green jobs for youths |
| • | AGM battery technology |
| • | Puerto Rico train stations |
| • | 2012 Energy Efficiency Forum |
| • | Automotive Interiors Awards |
| • | Hospital for Sick Children |
| • | World Environment Day |
| • | Start-Stop research |
| • | Best Corporate Citizens List |
What makes PowerFrame® different?
PowerFrame® grid technology is the advanced science on the inside of a battery that gives it the strength to withstand the elements outside. And the only way to know you’ve got True Strength™ on the inside of your battery is if it has the PowerFrame label on the outside.
The positive grid is the most important component of a battery. It’s what provides the energy to start your car - the backbone on which a battery is built. It’s also the part of the battery that most commonly leads to failure. Grid corrosion occurs over time as a result of the extreme temperature variations that batteries can experience. This corrosion weakens your battery and ultimately leads to failure.
That’s why PowerFrame’s smarter design, engineering and manufacturing set the standard.
PowerFrame grid technology is built with a sturdy outer frame which improves structural integrity to minimize corrosion and grid fractures.
The design of every PowerFrame grid optimizes the flow of electrons, which means you can count on your battery every time you need it.
But it’s not just what they’re made of that counts – it’s how they’re made. PowerFrame grids are made with a patented stamping technique that punches out the optimized and ideal pattern every time. The PowerFrame grid design is patterned for power and optimizes energy flow for consistent power over the life of the battery.
You can be confident that PowerFrame manufacturing is also environmentally friendly. The process is continuous and virtually waste-free, using 20% less energy and releasing 20% lower greenhouse gas emissions than other manufacturing methods.
PowerFrame’s performance has been tested and proven in the toughest real-world conditions imaginable: the extreme heat and stop-and-go driving environment of Las Vegas taxi cabs. Batteries with PowerFrame grid technology routinely outlast other batteries in head-to-head Las Vegas taxi-fleet studies.
The positive grid is the most important component of a battery. It’s what provides the energy to start your car - the backbone on which a battery is built. It’s also the part of the battery that most commonly leads to failure. Grid corrosion occurs over time as a result of the extreme temperature variations that batteries can experience. This corrosion weakens your battery and ultimately leads to failure.
That’s why PowerFrame’s smarter design, engineering and manufacturing set the standard.
PowerFrame grid technology is built with a sturdy outer frame which improves structural integrity to minimize corrosion and grid fractures.
The design of every PowerFrame grid optimizes the flow of electrons, which means you can count on your battery every time you need it.
But it’s not just what they’re made of that counts – it’s how they’re made. PowerFrame grids are made with a patented stamping technique that punches out the optimized and ideal pattern every time. The PowerFrame grid design is patterned for power and optimizes energy flow for consistent power over the life of the battery.
You can be confident that PowerFrame manufacturing is also environmentally friendly. The process is continuous and virtually waste-free, using 20% less energy and releasing 20% lower greenhouse gas emissions than other manufacturing methods.
PowerFrame’s performance has been tested and proven in the toughest real-world conditions imaginable: the extreme heat and stop-and-go driving environment of Las Vegas taxi cabs. Batteries with PowerFrame grid technology routinely outlast other batteries in head-to-head Las Vegas taxi-fleet studies.