Our Company
Our Businesses
Our Leaders
Our People
Our Diversity
Our Community Focus
Our Corporate Governance
Our History
Social Media
| ► | Company Profile |
| ► | Awards and Recognition |
| ► | Our Values |
| ▼ | Featured Stories |
| • | 2013 Edison Award |
| • | Automotive Innovations Award 2013 |
| • | Chery Jaguar Land Rover |
| • | Supporting Wounded Warriors |
| • | Auto Shanghai 2013 |
| • | 2013 Best Corporate Citizens |
| • | Diverse IT Professionals |
| • | Electronic Cockpit |
| • | 2012 Kepner-Tregoe Award |
| • | Diverse engineers |
| • | Bespoke Interior |
| • | Garbsen playground |
| • | Ethisphere 2013 |
| • | Hip-point mannequin |
| • | Junior Achievement |
| • | Better Buildings Challenge |
| • | Red Lion High School |
| • | Inspiration Seat |
| • | Governor's Ambassador Award |
| • | Sustainable Energy Factbook |
| • | Improving pediatric medicine |
| • | Hongqi H7 |
| • | Ford Fusion Auto Start-Stop |
| • | Compression Hybrid Molding |
| • | Micro Hybrid Battery |
| • | 2013 CES |
| • | Sound & Vibration Lab |
| • | Top Employer in China 2013 |
| • | Green Masters Program |
| • | Executive Involvement & Steering Program |
| • | Investor relations honors |
| • | Joint Center for Energy Storage Research |
| • | Holland battery plant |
| • | Journey from the heart |
| • | Red Cross Disaster Relief |
| • | Instituto Nacional de Cancerología |
| • | Blue Sky Involve |
| • | ÖkoGlobe 2012 |
| • | Corporation of the Year |
| • | Sustainability in the schools |
| • | Electric vehicle donation |
| • | Florence recycling facility |
| • | World Medical Relief |
| • | Innovative training |
| • | Safety first at Oak Ridge |
| • | Understanding Digital Natives |
| • | Chillers in mines |
| • | End-user research |
| • | Recycled resin |
| • | Green jobs for youths |
| • | AGM battery technology |
| • | Puerto Rico train stations |
| • | 2012 Energy Efficiency Forum |
| • | Automotive Interiors Awards |
| • | Hospital for Sick Children |
| • | World Environment Day |
| • | Start-Stop research |
| • | Best Corporate Citizens List |
The smart grid works, but only if smart buildings are connected to it. The time to do so is now.
The grid – the infrastructure that delivers electricity from power generating plants to buildings – is over-taxed. Because of increasing demand during peak time periods and the varying output of renewable energy sources such as solar and wind, the grid is less able to provide a stable energy supply.
However, by linking all supply and demand elements through intelligent two-way communication, the grid could constantly monitor demand and adjust delivery accordingly. That's the idea behind the "smart grid."
For example, by interfacing with home appliances or building controls, the smart grid could allow those energy-consuming devices to operate in off-peak periods and disable them during peak periods to save energy, reduce strain on the grid and enable users to consume electricity when it is least expensive.
To deliver all the benefits the smart grid has to offer requires that smart buildings be connected to it.
A smart building provides some or all of the following advanced capabilities:
However, by linking all supply and demand elements through intelligent two-way communication, the grid could constantly monitor demand and adjust delivery accordingly. That's the idea behind the "smart grid."
For example, by interfacing with home appliances or building controls, the smart grid could allow those energy-consuming devices to operate in off-peak periods and disable them during peak periods to save energy, reduce strain on the grid and enable users to consume electricity when it is least expensive.
To deliver all the benefits the smart grid has to offer requires that smart buildings be connected to it.
A smart building provides some or all of the following advanced capabilities:
- Optimized coordination of energy loads, on-site energy generation and energy storage
- Fully integrated control of lighting, heating, cooling, ventilation, IT, and other energy consuming systems, using weather data and information from security, scheduling and other business systems to optimize performance
- Advanced diagnostics and automated measurement, verification and reporting of energy and greenhouse gas emissions savings
- Continuous two-way communication between the building and the grid
- Automatic demand response to dynamic pricing signals from the grid
By utilizing smart building technologies, owners and tenants can vary electricity usage in response to signals from the grid when prices change to consume electricity when it's cheaper, and they can reduce demand when the grid is reaching capacity.
This is known as "demand response."
Smart building management systems can automate a short-term reduction in energy demand through load shedding or load shifting. For example, if the owner sets an electricity price threshold for the building and the grid signals that the price will exceed that threshold at a particular time of the day, the system would automatically reduce energy demand in the building at that time. The system could turn off non-critical loads, reduce lighting levels, let building temperatures float within limits or start the use of stored or on-site energy generation.
Combining smart grid and smart building technologies improves reliability and security, while reducing energy costs and greenhouse gas emissions.
Johnson Controls has been providing smart building technologies to customers for years and those customers are reaping the benefits.
Commercial buildings in the U.S. now consume 18 percent of the country's energy and 36 percent of the electricity. In a recent Energy Efficiency Indicator study, 44 percent of facility executives in the U.S. selected smart building technology as one of the top three technologies expected to have the greatest price-performance improvement over the next 10 years.
The time to deploy smart building technologies is now. Doing so could avoid $33 billion in energy costs and eliminate 160 million tons of carbon emissions annually by the year 2030.
This is known as "demand response."
Smart building management systems can automate a short-term reduction in energy demand through load shedding or load shifting. For example, if the owner sets an electricity price threshold for the building and the grid signals that the price will exceed that threshold at a particular time of the day, the system would automatically reduce energy demand in the building at that time. The system could turn off non-critical loads, reduce lighting levels, let building temperatures float within limits or start the use of stored or on-site energy generation.
Combining smart grid and smart building technologies improves reliability and security, while reducing energy costs and greenhouse gas emissions.
Johnson Controls has been providing smart building technologies to customers for years and those customers are reaping the benefits.
Commercial buildings in the U.S. now consume 18 percent of the country's energy and 36 percent of the electricity. In a recent Energy Efficiency Indicator study, 44 percent of facility executives in the U.S. selected smart building technology as one of the top three technologies expected to have the greatest price-performance improvement over the next 10 years.
The time to deploy smart building technologies is now. Doing so could avoid $33 billion in energy costs and eliminate 160 million tons of carbon emissions annually by the year 2030.
A DAY IN THE LIFE
ENERGY EFFICIENCY INDICATOR
Facility executives gave high marks to smart building technology in our latest study. more
MAKE YOUR BUILDINGS WORK
Explore our Web site to learn more about how Johnson Controls can help you enable your building to operate more efficiently, save energy costs, reduce carbon emissions, all while providing quality, productive, sustainable environments. more
INSTITUTE FOR BUILDING EFFICIENCY
The Institute for Building Efficiency is a new initiative of Johnson Controls providing information and analysis of technologies, policies, and practices for efficient, high performance buildings and smart energy systems around the world. more