Concept Cars
ie:3
As demonstrated throughout the ie:3, Inspired Efficiency moves beyond current knowledge and expectations to explore intriguing new possibilities.
re3
At North American International Auto Show 2009 in Detroit Johnson Controls introduced re3.
i3 (2007)
The alignment of the interior to the needs of the driver played a particularly important role in the i3 interior demonstrator which was introduced at the IAA in Frankfurt in 2007.
Mesos (2006)
At the 2006 North American International Auto Show in Detroit, USA, Johnson Controls introduced an Electronics Innovation Vehicle called Mesos, presenting a range of up to date solutions in electronics.
Ikanos (2005)
First unveiled at the 2005 North American International Auto Show, the Ikanos concept interior presented applications of Johnson Controls’ interior technologies – both current and in-development.
3e (2004)
Everyday Needs - the interior concept 3e responded to emerging priorities through a cross-section of generations - created for the 2004 North American International Auto Show.
Ariston (2001)
Ariston was created on the occasion of the 2001 North American International Auto Show. Ariston combined luxury and personalization options in the automotive interior.
Etimos (2001)
Etimos was created in 2001 for the IAA in Frankfurt. The seamless interplay of technology and design reflected the consumer’s new awareness of comfort, functionality and driving pleasure.
Kion (2000)
In the year 2000, the Kion concept car was introduced at the Mondial de l'Automobile in Paris to present the automotive interior as the intelligent living space of the future.
Vios (1999)
Vios with its flexible, custom-made concept for the small segment car was introduced at the 1999 IAA in Frankfurt.
ESV (1998)
The ESV (European Show Vehicle) from Johnson Controls demonstrated in 1998 how automobile travel can be made even more pleasant in the future.
Symbiosis (1997)
At the 1997 IAA in Frankfurt Johnson Controls introduced a concept interior called Symbiosis, presenting a totally harmonious, near-future interior that emphasizes aesthetic appeal, practical elegance and value.