Automotive Experience
Solingen Development Center
With the purchase of C. Rob. Hammerstein GmbH and KEIPER GmbH in spring 2011 Johnson Controls Automotive Experience has expanded its range in developing complex metal seating structures and components.
One of the development centers in the Product Business Unit Metals covering about 97,000 square feet is located in Solingen, not far from the European Headquarters in Burscheid. More than 500 employees working on product development, program management, benchmarking, prototype construction and acoustic research for development, sales and other central functions are currently located there.
The development center is close to the production plant in the suburb of Ohligs and therefore provides quick communication with production. The Solingen location is directly connected with the cities of Cologne and Düsseldorf via the A3 highway.