Automotive Seating
Automotive Interiors
Automotive Electronics
Our Approach
Awards
Featured Stories
Open Innovation
Supplier Information
| ► | Global Leadership |
| ► | Customers & Sales |
| ► | Core Product Portfolio |
| ► | Safety & Comfort |
| ► | Best Business Practices |
| ► | Industrial Design and Human Factors |
| ► | Product and Systems Engineering |
| ▼ | Research & Testing |
| • | Consumer Research |
| • | Acoustics |
| • | RF TestLab |
| ► | Craftsmanship |
| ► | Materials & Environment |
| ► | Integrated Interiors |
A Sound Investment for our Customers: The Johnson Controls’ Radio Frequency Test Lab
As the number of Radio Frequency (RF)-based devices in automobiles increases, our job is to decrease the potential they represent for creating electronic noise or interference.
Johnson Controls’ initiatives to advance and improve the testing of radio-frequency signals in vehicle interiors have resulted in the automotive industry's first and only year-round, Federal Communications Commission (FCC)-certified, vehicle-level RF testing facility.This test site allows us to maximize the reliability and accuracy of our current RF products, such as the HomeLink® Wireless Control System and our Blue Connect™ Bluetooth enabled Telematics Hands-Free System. The facility will also continue to play a key role in the development of new electronic products and features.
RF Test Lab Features:
- Certified 3- and 10-meter testing in a completely enclosed facility that provides year-round accessibility
- FCC-certified for vehicle-level testing, in addition to module-level testing
- Only enclosed 10-meter site with an extended range-test capability of up to 100 meters
As demonstrated throughout our new demonstrator ie:3, Inspired Efficiency moves beyond current knowledge and expectations to explore intriguing new possibilities.
We operate several development centers around the world with dedicated space to develop state-of-the-art product technologies.