29-Palms-solar-image

Solar Photovoltaic Energy

Solar electrical energy is generated when the sun’s energy strikes a solar photovoltaic (PV) panel. A series of PV panels are combined in PV arrays that send Direct Current (DC) to an inverter, which converts the electricity to Alternating Current (AC) Power. The AC power is integrated into the building’s electrical system, thereby reducing the amount of electricity that must be purchased from the grid. Solar PV systems can be sized to produce as much or as little power that is required in a given application.

 

We partner with you to take responsibility for all areas of a project including design, financing, operations and maintenance of your system.

 

We are partnering with:

  • Federal agencies
  • Military installations
  • State and local government
  • K-12 schools
  • Colleges and universities
  • Hospitals and healthcare organizations
  • Commercial real estate
  • Warehouse,  manufacturing sites
  • Public housing