YORK® Water-Cooled Absorption Chillers

With more than 40 years of experience, YORK® water-cooled absorption chillers are highly reliable machines that are powered by steam, hot water, or natural gas. YORK® water-cooled absorption units range from 120 to 1,380 Tons of Refrigeration (420-4,850 kW)
YIA Water-Cooled Single-Stage Absorption Chiller


The YORK® YIA water-cooled single-stage absorption chiller offers increased reliability and enhanced performance.

YPC Water-Cooled Two-Stage Absorption Chiller

 

The YORK® YPC water-cooled two-stage absorption chiller represents the world’s most efficient commercially available absorption technology.