Air Measuring

Requirements to monitor the air flow into and within a building have increased over the years with the IAQ requirements for minimum ventilation of occupied spaces. There are two methods by which air flow is measured within a duct:
AD-1250sm
Differential Pressure which has been available since the days of pneumatic control
AD1252sm

Thermal Dispersion which has been available about 10 years