yvwaBanner

Delivering Efficiency, Flexibility, Sustainability and Confidence with Cutting-edge Design

The new YORK® YVWA water-cooled screw chiller helps building owners and designers achieve their goals while cutting energy and carbon emissions by as much as 30 percent.

We've taken water-cooled screw chiller efficiencies to a whole new level.

The new YORK YVWA water-cooled screw chiller uses a number of engineering advances to address four primary requirements of building owners and designers — efficiency, application flexibility, sustainability, and confidence.

  • Efficiency: The variable-speed drive saves energy during the 99 percent of operating hours spent at off-design conditions, when building loads and/or tower-water temperatures are lower. As a result, the YVWA delivers an Integrated Part Load Value (IPLV) as much as 30 percent better than traditional screw chillers, making it best-in-class.

  • Flexibility: Because the YVWA screw chiller is capable of handling a higher pressure lift than a centrifugal chiller, it can be used in both thermal-storage and heat-pump applications, while delivering the highest efficiencies available. This remarkable flexibility also allows the chiller to utilize a wide range of heat-rejection methods, including an open cooling tower, dry cooler, adiabatic cooler, heat recovery, or heat pump.

  • Sustainability: The YVWA chiller does not make you choose between saving money and saving the environment. The YVWA chiller reduces environmental impact in two ways:
  1. Directly, by managing refrigerant charges and the potential refrigerant leak points
  2. Indirectly, by minimizing power-plant CO2 emissions, which are responsible for 98% of the Global Warming Potential associated with chillers

  • Confidence: Gain confidence by partnering with the experts. Johnson Controls invented variable-speed-drive technology for water cooled chillers in 1979. We also introduced the industry’s first variable-speed, air-cooled, screw chiller in 2004. By 2010, our installed base exceeded 2,500,000 TR in over 100 countries. With all units combined, we have more than 20,000 years of field experience. 

Learn more about the new YORK YVWA chiller or locate your nearest Johnson Controls sales representative on our web site.