Integrated HVAC Systems
Building Management Systems
Security & Fire Safety Solutions
Technical Building Services
Commercial Refrigeration
Industrial Refrigeration
Global WorkPlace Solutions
Energy Efficiency & Sustainability
Solutions For Your Building
Global Marine and Navy
Efficiency Now Newsletter
HVAC Training Resources
Case Studies
| ► | May 2013 |
| ► | March 2013 |
| ► | February 2013 |
| ► | January 2013 |
| ► | November 2012 |
| ► | September 2012 |
| ► | July 2012 |
| ► | June 2012 |
| ► | May 2012 |
| ► | April 2012 |
| ► | March 2012 |
| ► | February 2012 |
| ▼ | January 2012 |
| • | Fort Bliss |
| • | Waldo County General Hospital |
| • | Bowie State |
| ► | November 2011 |
| ► | October 2011 |
| ► | September 2011 |
| ► | July 2011 |
| ► | June 2011 |
| ► | May 2011 |
| ► | April 2011 |
| ► | eNewsletter Opt In |
Maine Hospital Finds Relief, Energy Efficiency and Savings with New Chillers
Utility savings and incentive allow community hospital to achieve an amazing four-year return on investment
When Maine’s Waldo County General Hospital found its chiller was ailing, they sought a cure that would bring them reliable comfort for patients and staff, improved energy efficiency and a level of redundancy that would maintain a healthy environment at all times. The not-for-profit community hospital also needed a cost-effective replacement that would continue to contribute to a vigorous bottom line. Johnson Controls proposed a double chiller replacement that will save an estimated $47,785 annually in electricity costs, provide reliable cooling and achieve a four-year return on investment.
After conducting a study of the hospital’s cooling needs, the Johnson Controls service team proposed a solution that would not only meet the hospital’s requirements, but also reduce future costs and eliminate the environmentally unfriendly refrigerant used in the existing chiller. In addition, Johnson Controls leveraged available funding to offset the cost of the project itself.
Solution includes hardware, software and financial incentives
Johnson Controls replaced the aging 270-ton chiller with two 150-ton chillers equipped with variable speed drives, which operate far more efficiently. The two chillers ensure that critical patient care areas will remain cool if a problem occurs with one of the chillers. Johnson Controls also expanded the hospital’s Metasys building management system, allowing the system to easily switch the cooling load from one chiller to the other, saving energy and maximizing the life of the chillers. The old unit ran around the clock for up to 10 months of the year, an excessive amount that meant costly repairs each year on the unit’s compressors.
Not only do the new chillers use a more environmentally friendly R134a refrigerant, they also run much more efficiently. The hospital is expected to save about $47,785 a year in electricity costs. In addition, Johnson Controls worked with Efficiency Maine – a program that provides incentives and grants to help residents and businesses reduce energy costs – to secure a custom incentive of $142,000. Johnson Controls used YORKcalcTM modeling software to build a performance profile and project savings to help in determining the amount of the incentive.
Thanks to reduced electricity costs, the incentive, and the maintenance savings, the new chillers are expected to pay for themselves in less than four years. After that point, the new chillers will continue to generate significant savings that will offset future utility and other operational costs. The two chillers’ additional 30 tons of capacity will allow for future hospital growth as well.
Critical care maintains comfort and smooth operations
Replacing a chiller is a delicate procedure in a 24/7 care environment like a hospital. To minimize downtime and disruption to the facility, Johnson Controls performed a two-stage operation. With the old unit still in service, one new chiller was lifted to the hospital roof, installed and started. At a later date, the old unit was removed and the second chiller was lifted to the roof and installed, and the new unit brought online. Because of careful planning and efficient service – including a 4 a.m. start time – the building temperature rose only a few degrees during the four-hour cutover period to the new system.
After conducting a study of the hospital’s cooling needs, the Johnson Controls service team proposed a solution that would not only meet the hospital’s requirements, but also reduce future costs and eliminate the environmentally unfriendly refrigerant used in the existing chiller. In addition, Johnson Controls leveraged available funding to offset the cost of the project itself.
Solution includes hardware, software and financial incentives
Johnson Controls replaced the aging 270-ton chiller with two 150-ton chillers equipped with variable speed drives, which operate far more efficiently. The two chillers ensure that critical patient care areas will remain cool if a problem occurs with one of the chillers. Johnson Controls also expanded the hospital’s Metasys building management system, allowing the system to easily switch the cooling load from one chiller to the other, saving energy and maximizing the life of the chillers. The old unit ran around the clock for up to 10 months of the year, an excessive amount that meant costly repairs each year on the unit’s compressors.
Not only do the new chillers use a more environmentally friendly R134a refrigerant, they also run much more efficiently. The hospital is expected to save about $47,785 a year in electricity costs. In addition, Johnson Controls worked with Efficiency Maine – a program that provides incentives and grants to help residents and businesses reduce energy costs – to secure a custom incentive of $142,000. Johnson Controls used YORKcalcTM modeling software to build a performance profile and project savings to help in determining the amount of the incentive.
Thanks to reduced electricity costs, the incentive, and the maintenance savings, the new chillers are expected to pay for themselves in less than four years. After that point, the new chillers will continue to generate significant savings that will offset future utility and other operational costs. The two chillers’ additional 30 tons of capacity will allow for future hospital growth as well.
Critical care maintains comfort and smooth operations
Replacing a chiller is a delicate procedure in a 24/7 care environment like a hospital. To minimize downtime and disruption to the facility, Johnson Controls performed a two-stage operation. With the old unit still in service, one new chiller was lifted to the hospital roof, installed and started. At a later date, the old unit was removed and the second chiller was lifted to the roof and installed, and the new unit brought online. Because of careful planning and efficient service – including a 4 a.m. start time – the building temperature rose only a few degrees during the four-hour cutover period to the new system.
INSTITUTE FOR BUILDING EFFICIENCY
Read What’s New for IBE
Our easy-to-use Energy Efficiency Calculator lets you estimate energy cost savings, improve productivity, and reduce carbon emissions through building improvements.
Waldo County General Hospital