X Close
Self-Paced HVAC and BAS Courses
Convenient, effective and portable learning materials
Interactive CD-ROMs, instructional videotapes and self-study workbooks offer flexible, effective, cost-efficient opportunities to build knowledge and skills. Learn in the convenience of your own home, office or work location using Johnson Controls Training Institute Learning Packages.

Computer-Based Training

Product CBT22
Using PMI on the Metasys Operator Workstation
, Price $395
This updated (PMI Rev.11) interactive computer-based training program will introduce you to basic operation of the Metasys® PMI feature-set. Hands-on practice in a simulated PMI environment is part of each lesson in this module. A "Tell Me" explanation and "Show Me" demonstration video of each procedure is also included. Its modular construction means you can take topics in the order in which you need or desire them! Twenty-five topics are organized into five lessons.
Order Form


Product C-3100-EN
Application and Installation of Controls for Commercial Comfort Systems
, Price $99
This two part, computer based course builds knowledge and skill in both the application and installation of controls for Commercial Comfort Systems. This interactive learning experience will help you properly apply these controls to the various types of HVAC systems. Also, this experience will help you install the system through proper planning, layout of control and network devices, mounting, wiring and cabling, terminating, addressing and balancing of the system. The primary audience for this learning is electrical installation personnel who install the system. The secondary audience includes mechanical personnel who may troubleshoot the system. Basic understanding of HVAC and control systems is recommended.
Order Form


Product CBT7500
Building Automation System Networking, Price $195
Build your knowledge, comprehension and vocabulary about basic networking concepts and technology. This learning experience will help you to connect networking equipment to devices; determine the appropriate use of hubs, repeaters, switches and bridges on a Metasys® network; verify that your Metasys® network is properly configured, and configure a remote communications device. Before beginning this learning package, it would be helpful to be familiar with the components, terminology and characteristics of a Metasys® network, including the purpose of a supervisory controller and the concepts of the Metasys® N1 LAN, N2 Bus, L2 Bus and S2 Bus. 
Order Form


Product LM17
HVAC Introduction
, Price $99
Explore the fundamental concepts, theories and principles of the building environment industry in this comprehensive introduction to HVAC Systems and controls. This interactive CD-ROM focuses on the relationships among environmental requirements, building mechanical systems, and the controls that regulate mechanical systems. The built-in tracking system will help individual users keep track of what they have covered and the test scores they have achieved. The accompanying workbook provides much more than just a place to record notes -- it contains questions to prompt critical thinking, review and application of the concepts presented online.
Order Form


DVDs

Product P55
HVAC System Types
, Price $195

Color animated graphics and views of actual HVAC system components provide an in-depth study of the three ASHRAE classifications: all water, all air and air-water HVAC systems. This two-part learning package explains the differences between the various types of HVAC systems, including the advantages, disadvantages and common applications for each type. The clearly written materials also describe the different control strategies used to control temperature and relative humidity. 
Order Form


Written Material

Product P55
HVAC System Types
, Price $195
Color animated graphics and views of actual HVAC system components provide an in-depth study of the three ASHRAE classifications: all water, all air and air-water HVAC systems. This two-part learning package explains the differences between the various types of HVAC systems, including the advantages, disadvantages and common applications for each type. The clearly written materials also describe the different control strategies used to control temperature and relative humidity. 
Order Form


Product P99
Building Environments: HVAC Systems
, Price $49.95
Creating healthy, productive indoor environments can be the greatest challenge facing those involved with buildings. This comprehensive, easy-to-read text builds your understanding of HVAC systems and the controls that manage them. More than 270 supporting illustrations and examples explain how mechanical and control systems work together to create quality building environments. Learn the technical details behind these complex systems without being overwhelmed!
Order Form


Product P2074
HVAC Controls Manual
, Price $30
This handy reference provides a clear, concise explanation of the application of pneumatic controls to HVAC systems.Fundamental HVAC concepts, such as the components of a control system, master/submaster theory, and the role of auxiliary devices, are covered in an easy-to-read format. A comprehensive exam at the back of the book checks the student’s understanding of the material. 
Order Form