X Close
Kokomo Improves Quality of Life for Citizens in Need
Innovative Financing Model Helps Improve Quality of Life for disadvantaged citizens.
Share On
Share
Challenge
The Housing Authority of the City of Kokomo offers affordable, safe, sanitary housing for low-income individuals and families. The organization relies heavily on federal funding to operate and maintain 550 units across multiple sites within the city. And like many federally funded groups, the housing authority has been forced to do more with less in recent years. 
 
“The funding has been shrinking,” said CEO Deb Cook. “Every agency is challenged, but HUD (Housing and Urban Development) has been hit extremely hard, and we’ve just tried to make do and put out fires as best we can.” Many of the city’s facilities were in desperate need of infrastructure improvements - roofs, siding, plumbing, heating and lighting.
Solution
The Johnson Controls team designed a plan that would include $3.3 million in upgrades and repairs across the housing units, paid for from energy savings and HUD incentives, without the need for the Kokomo Housing Authority to provide capital.
 
Under an energy savings performance contract, improvements would be paid for up front by Johnson Controls and guaranteed to generate enough savings to pay for themselves over time. “We considered energy performance contracting a few years ago but back then you had to repay the loan from capital funds which, for us, were shrinking,” said Director of Finance Debbie Stapleton. “Today, we have more options and Johnson Controls showed us how the energy and water savings could be used to pay back the loan. So this is the first time we were able to seriously consider it as a solution.”
Results
With the funding mechanism in place, the project got underway in 2013 and included water conservation efforts, bath-to-shower conversions, lighting upgrades, HVAC upgrades, new sliding doors, weatherization and other initiatives designed to improve energy efficiency and provide a more comfortable, safe and secure environment for residents through:
  • Reduced energy use: The performance contract guarantees $223,000 in annual energy savings with a payback term of 20 years.
  • Reduced water use: With the installation of new fixtures and the conversion of tubs to showers in one building, water savings reached $133,000 in just six months.
  • Improved lighting: New lighting in hallways, parking lots and other outdoor areas not only contributes to the energy savings, it gives housing authority residents a greater sense of security.
 
In addition to the results guaranteed in the energy savings performance contract, the project had a positive impact on the broader community, through:
  • Job creation: 70% of the contractors working on the project were local.
  • Job training: As a recipient of HUD financial assistance, the city of Kokomo was required to provide training, employment, and contracting opportunities for low- or very-low income residents in connection with the project. A two-week job-skills training program was held for interested members of the community.
  • Lender participation: The project utilized a local financial lender.
 
Share On
Share

Related Case Studies

Hawaii
The Hawaii Department of Transportation takes unprecedented steps to improve airports, highways and harbors
Hawaii’s Department of Transportation entered a strategic and technical partnership with Johnson Controls.
Greening Louisville
Johnson Controls was part of the team implementing Louisville’s first comprehensive sustainability plan, becoming one of the greenest cities in the country. That’s despite inefficient, high-maintenance building equipment decades past its life expectancy. The $27 million approach to energy efficient upgrades and repairs in 200 municipal-owned buildings was done without the need for Louisville Metro to provide capital or assume financial risk.