This site uses cookies to offer you a better browsing experience. By continuing to navigate through this site or by clicking Approve, you consent to the use of cookies on your device as described in our privacy notice.
How can we make our cities more sustainable?

Thoughts by Chairman and CEO Alex Molinaroli
Urbanization continues to spread globally, with 70 percent of the world’s population expected to live in cities by 2030. This trend brings with it the urgent need for more efficient use of energy, cleaner energy generation and cost effective energy storage. While the public sector must lead, it should work closely with the private sector to rapidly implement best practice policies, programs and projects that will improve urban efficiency and sustainability.

Best practices for improving building energy efficiency in cities include: 1) adopting and enforcing building codes and appliance standards; 2) setting reduction targets and adopting sustainable construction and leasing policies; 3) establishing retrofit programs for public and private sector buildings; 4) introducing certification, benchmarking and transparency programs; 5) accepting innovative financial models and programs; and 6) coordinating efforts with local utilities. While results are promising, very few cities globally have implemented a comprehensive set of these elements.
To help cities, the World Resources Institute (WRI), the United Nations Environment Programme (UNEP) and the Global Environment Facility announced the expansion of the Building Efficiency Accelerator during Paris COP-21. The Building Efficiency Accelerator is a partnership between WRI, the UN Sustainable Energy for All (SE4ALL) initiative and other organizations and industry partners including ICLEI, Global Green Growth Forum, Johnson Controls and Ingersoll-Rand. This program focused on doubling the rate of global energy efficiency improvement emerged from an initial dialogue at the 2014 Annual Meeting in Davos.
One early engagement of the Building Efficiency Accelerator is in Mexico City. Mayor Mancera announced on Buildings Day during COP-21 that Mexico City plans to integrate building energy performance in local construction codes, retrofitting hospitals with solar hot water and efficiency measures, and auditing and retrofitting municipal buildings. A launch event in March included over 100 participants from city and federal government and the private sector. The engagement is now being supported by four working groups chaired by Mexico City staff and managed by WRI/CTS EMBARQ.
"Increasing urban efficiency must be a priority for leaders at all levels as we collectively strive to promote the quality of life for city residents."
-- Johnson Controls Chairman and CEO Alex Molinaroli
While buildings represent a great opportunity to improve demand-side urban efficiency, district energy systems are seeing a resurgence of interest in urban sustainability on the supply side. Modern district energy systems provide centralized heating and cooling to urban areas with efficiency gains of up to 80-90 percent over conventional solutions.Paris initially developed a district heating system in 1927 to reduce air pollution from burning coal. Today, renewables provide more than 50 percent of co-generated heat to the equivalent of 500,000 households. Paris also developed Europe’s first and largest district cooling system using water from River Seine while improving energy efficiency by 35 percent.
The UN SE4ALL District Energy Accelerator builds upon the success of the UNEP District Energy in Cities initiative which has documented best practices from 65 cities around the world. The District Energy Accelerator includes many institutional and industry partners including ICLEI, UN Habitat, Danfoss and Veolia.
In Dubai, air conditioning represents 70 percent of electricity consumption. The city is developing the world's largest district cooling network which will cut this electricity use in half while also reducing its consumption of fresh water through use of treated sewage effluent. The city of Anshan, China is integrating isolated boilers into their district heating network and capturing waste heat resulting in a 1.2 million ton reduction in annual coal use. Finally, Tokyo is capturing waste heat from buildings and metro stations, heat pumps connected to local water sources and solar thermal energy
Stanford University has implemented an innovative strategy for building energy efficiency and modern district energy technology. Driven by the State of California’s aggressive goals to reduce greenhouse gas emissions and water consumption, the university developed a plan to reduce building energy use by up to 30% less than code, increase renewable energy generation to 73 MW, decommission an existing natural gas fired combined heat and power plant and build a new water- and energy-efficient central energy system. The new energy system provides 90% of campus heating needs from heat recovery chillers and reduces water consumption by 15%. The design includes chilled and hot water storage systems managed by sophisticated predictive control algorithms that forecast weather conditions, campus energy requirements and energy costs ten days in advance.
Increasing urban efficiency must be a priority for leaders at all levels as we collectively strive to promote the quality of life for city residents and address the great challenges of global climate change, energy security and economic development. A number of global partnerships are helping build capability and capacity through increased collaboration between the public and private sectors. With record numbers of cities, businesses and institutions making ambitious commitments during Paris COP-21, now is the time to leverage the experience, resources and solutions of the private sector combined with the leadership of local governments to accelerate action towards urban efficiency and sustainability.