Consumers Digest recognizes York® gas furnaces for energy efficiency and cost savings

Share On
Share

Two York® Affinity™ modulating gas furnaces win Best Buy awards

MILWAUKEE – (September 22, 2014) – Consumers Digest recently named Johnson Controls Best Buy award winners for two York® Affinity™ Series modulating gas furnaces models for outstanding efficiency ratings,  fuel-conserving features and improved homeowner comfort. The designation also considered ease of use, maintenance requirements and quality and reliability.

The variable-speed model features an electronically commutated motor (ECM) that delivers up to 98 percent Annual Fuel Utilization Efficiency (AFUE), positioning the unit among the industry’s most efficient gas furnaces. The second Affinity model recognized by Consumers Digest uses a permanent split capacitor (PSC) motor to deliver a 97 percent AFUE.

“For dealers and homeowners searching for efficient heating systems that are easy to install and service in tight spaces while contributing to sustainable home design, the York Affinity furnaces are a great choice,” said Liz Haggerty, vice president and general manager, Unitary Products Group, Johnson Controls.

Both units are conveniently compact and stand at just 33 inches, making them the ideal solution for applications where space is limited, including closets, attics and basements with low ceilings. Homeowners who install one of the furnaces in their homes will also appreciate the unit’s quiet operation.

These York Affinity furnaces are ENERGY STAR® qualified and come with a lifetime limited warranty on the heat exchanger from Johnson Controls. All other model components include a 10-year limited warranty.

York  products from Johnson Controls include energy-efficient, residential central air conditioners, heat pumps, furnaces and accessories and innovative light-commercial, packaged heating and cooling systems marketed through a national distribution network and delivered to home- and building-owners through qualified York heating and cooling contractors. For more information about York, visit: www.york.com.

Follow us at @JCI_BEnews

Visit www.johnsoncontrols.com/benews

 

About Johnson Controls

Johnson Controls is a global diversified technology and industrial leader serving customers in more than 150 countries. Our 170,000 employees create quality products, services and solutions to optimize energy and operational efficiencies of buildings; lead-acid automotive batteries and advanced batteries for hybrid and electric vehicles; and interior systems for automobiles. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. Through our growth strategies and by increasing market share we are committed to delivering value to shareholders and making our customers successful. In 2014, Corporate Responsibility Magazine recognized Johnson Controls as the #12 company in its annual “100 Best Corporate Citizens” list. For additional information, please visit http://www.johnsoncontrols.com or follow @johnsoncontrols on Twitter.

# # #

Share On
Share