YORK®, winner of Trusted Brand Award, unveils unmatched product range to cool more Malaysians using less energy

Share On
Share

Johnson Controls’ building solutions and services meet diverse customer needs for residential, commercial and industrial applications


PETALING JAYA, Malaysia – May 25, 2016 – YORK®, winner of the Trusted Brand Award, showcases its unmatched portfolio of Heating, Ventilation, Air-conditioning and Refrigeration (HVACR) products to meet the diverse cooling needs and budgets of customers in Malaysia at optimal energy efficiency.

The range on display at REVAC 2016, one of Southeast Asia’s largest HVACR events, includes:

  • Variable Refrigerant Flow (VRF) systems with capacities of 4 (3 kW) to 54 HP (40 kW) and high Coefficient of Performance[1] (COP) of up to 4;
  • Water-cooled screw chillers with capacity ranging between 97 tons (340 kW) to 433 tons (1,500 kW) with COP as high as 6.37 and Integrated Part Load Value[2] (IPLV) of up to 9.56 for some of the models;
  • High-end YMC2 with capacity of up to 1,000 tons (3,500 kW), capable of achieving IPLV of more than 11.

Johnson Controls is pushing the technical front on advanced chillers with YMC2. The chiller uses magnetic levitation technology – first applied by the company in mission-critical nuclear submarines – in its driveline to spin without friction. This not only results in extremely high energy efficiency and ultra-quiet operation of 70 dBA; its fewer moving parts also means less servicing, longer motor life and greater reliability. 

Apart from being a technology leader, YORK is also a market leader in Malaysia’s HVACR sector. From large tonnage chillers for complex applications to environmentally-friendly five-star energy-efficient products for residences, YORK has a strong track record in Malaysia.

 “YORK instills confidence and is trusted in Malaysia, having been in this country since 1978 and having cooled some of Malaysia’s most iconic buildings including Kuala Lumpur International Airport 2, Pavilion and Mid Valley City. So I am really pleased to announce today that we have been honored with the Trusted Brand Award by Reader’s Digest for the 13th consecutive year,” said Douglas Toh, general manager of products distribution, Building Efficiency Malaysia, Johnson Controls. The Award is based on a survey with ordinary consumers on what brands are important to them.

To help customers select the system that best delivers energy efficiency at the best price point while lowering life-cycle cost, Johnson Controls experts can guide customers through a thorough analysis. Furthermore, the company also offers airside products and Metasys® building automation systems that integrate well with its HVACR products.

“This is where the sum is more than its parts. We want to give our customers the best value and experience through a convenient, one-stop reference point for building solutions and services. With a response time of not more than four hours, our service standards are one of the highest in the industry,” said Ken Lim, general manager, Building Efficiency Malaysia, Johnson Controls.

[1] COP is a measure of the ratio of cooling output to electrical power input at full load.

[2] IPLV is the measure of ratio of cooling output to electrical power input at various operating capacities.

About Johnson Controls

Johnson Controls is a global diversified technology and industrial leader serving customers in more than 150 countries. Our 150,000 employees create quality products, services and solutions to optimize energy and operational efficiencies of buildings; lead-acid automotive batteries and advanced batteries for hybrid and electric vehicles; and seating components and systems for automobiles. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. Through our growth strategies and by increasing market share we are committed to delivering value to shareholders and making our customers successful. In 2016, Corporate Responsibility Magazine recognized Johnson Controls as the #17 company in its annual “100 Best Corporate Citizens” list. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

About Johnson Controls’ Building Efficiency

Johnson Controls’ Building Efficiency has an unmatched portfolio of HVACR products and solutions to create more comfortable, safe and efficient buildings. Operating in more than 150 countries through a strong network of distribution channels, Building Efficiency’s breadth of offerings helps building owners, operators, engineers and consultants impact the full lifecycle of a building. Its market leadership is established through trusted brands such as YORK®, Sabroe® and Metasys® as well as its smart building integration capabilities and energy financing solutions. For more information, visit http://www.johnsoncontrols.com or follow @JCI_BEnews.

 

# # #

CONTACT:     Ngiam Shing Shian

Regional Communications Manager (Asia Pacific)

Building Efficiency, Johnson Controls

Work + 65 6854 8643

Mobile + 65 9620 9561
            shingshian.ngiam@jci.com


Share On
Share