Johnson Controls introduces Verasys™ controls system, first plug-and-play solution that integrates HVACR equipment and controls

Share On
Share

Flexible solution ensures low field installation costs and new level of insight into building operations

MILWAUKEE – (Jan. 5, 2017) – Johnson Controls introduces Verasys™, the first plug-and-play controls system that integrates heating, ventilation, air-conditioning and refrigeration (HVACR) equipment and controls.

Verasys offers customers in the light commercial market a flexible, one-source procurement solution with advanced technology already embedded for the self-discovery of Smart Equipment™. Suitable for single- or multi-zone applications, the new controls system seamlessly connects to a vast range of mechanical and electrical equipment, controls and sensors using wireless configurations that result in cost savings. Verasys accomplishes this without requiring any special programming tools, ensuring low installation costs.

Verasys equips contractors with a complete solution

Configurable controllers provide simple settings for implementation, but contractors have the option to change defaults to meet their unique requirements. Verasys also empowers them to offer a complete bundled solution of Smart Equipment and controls that work with third-party, package equipment for greater application, flexibility and protection of existing investments. And because the system communicates using BACnet® MSTP, Verasys integrates with Metasys® or any third-party BACnet system. Contractors will also appreciate new opportunities to service equipment, thanks to optional fault detection and diagnostics that immediately deliver alarm notifications via email or text.

Building operators experience unprecedented access to information

For building operators, Verasys provides unprecedented, remote access anytime, anywhere over a secure internet connection using PCs, smartphones and tablets. The controls system connects users to data streams from smart controls in rooftop units, fan coils, zone dampers, heat pumps, refrigeration systems, lighting panels and more. With real-time data, building operators can identify and troubleshoot issues remotely and take advantage of insightful solutions that deliver the quality and value their facilities require.

Building operators will also appreciate simple graphics that provide fast access to information, enabling them to take advantage of a new level of insight into building operations. Immediate access to critical information ensures energy efficiency and lower operating costs throughout a building’s life cycle. Users can identify issues before they result in unplanned downtime, and equipment life is extended. The advanced level of control flexibility, including scheduling, alarming, setpoints and more, also saves time, increases productivity and results in facilities that better serve occupants.

To learn more about Verasys from Johnson Controls, visit www.verasyscontrols.com.

 

About Johnson Controls

Johnson Controls is a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries. Our 135,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

About Johnson Controls’ Building Technologies & Solutions

Johnson Controls’ Building Technologies & Solutions has an unmatched portfolio of HVACR products and solutions to create more comfortable, safe and efficient buildings. Operating in more than 150 countries through a strong network of distribution channels, Building Technologies & Solutions’ breadth of offerings help building owners, operators, engineers and consultants impact the full lifecycle of a building. Its market leadership is established through trusted brands such as YORK®, Sabroe® and Metasys® as well as its smart building integration capabilities and energy financing solutions. For more information, visit www.johnsoncontrols.com or follow @JCI_BEnews.

 

# # #

CONTACT:  

   

Ryan Nolan

Public Relations Program Manager

Building Technologies & Solutions, Johnson Controls

Work + 1 414 524 6170

Mobile + 1 414 378 9641

Ryan.P.Nolan@jci.com

Share On
Share