Johnson Controls unveils new Vertical Stacked Water Source Heat Pump Sound Room

Share On
Share

Customers can experience best-in-class water-source heat pump sound performance in a residential setting

MILWAUKEE – (Oct. 17, 2017) – Johnson Controls today unveiled its new Vertical Stacked Water-Source Heat Pump Sound Room in Ajax, Ontario, Canada. The Sound Room contains two working Johnson Controls vertical stacked water-source heat pump (VS-WSHP) units, allowing customers to experience first-hand the best-in-class sound performance of the high-efficiency 13 EER model and the premium-efficiency 16 EER model in a residential setting.

“Johnson Controls is the only manufacturer to offer two performance platforms for water-source heat pumps,” said Karl Washburn, principal engineer, acoustics, Building Technologies & Solutions at Johnson Controls. “Both units are engineered and manufactured to minimize noise and have undergone independent sound testing according to AHRI 260. The new Sound Room complements our recently released Sound Application Guide for the vertical stacked heat pump and gives customers the opportunity to listen to the units before purchasing them.”

The quiet operation of VS-WSHPs can be attributed to cabinets that are isolated from the wall structure to prevent vibration and noise transmission. The optional isolated chassis further reduces noise and vibration to contribute to a quieter, more comfortable environment for occupants and a more marketable facility for building owners.

Designed to replicate a room in a condominium, the 250-square-foot Sound Room demonstrates one of several applications for VS-WSHPs that also include high-rise apartments, dormitories, renovated office space, assisted living communities and other multi-story buildings with repeating floor patterns, as well as the replacement market.

“High-rise construction, whether two stories or twenty stories, presents unique HVAC challenges,” said Dan Tyson, product manager, Indoor Packaged Equipment (IPE), Johnson Controls. “The challenge is to maximize floor space for occupants and still create efficiencies during and after construction. Our vertical stacked heat pumps feature design and construction details that provide the flexibility you need—things like a compact footprint, the flexibility and comfort of a four-pipe fan coil system at the cost of a two-pipe system, optional individual tenant metering and easy service access.”
"Johnson Controls is the only manufacturer to offer two performance platforms for water-source heat pumps." -- Karl Washburn, principal engineer, acoustics, Building Technologies & Solutions at Johnson Controls.

Johnson Controls VS-WSHPs also deliver total system efficiency with energy recovery for heating, cooling, humidifying and dehumidifying. For additional operating efficiency, the units offer fully integrated digital controls featuring BACnet®, MS/TP and LON® protocols and seamless BAS integration. And because water transfers heat more efficiently, the water-source heat pumps are the ideal solution for water-loop and geothermal applications, reducing energy costs up to 50 percent, when compared to conventional cooling and heating systems. Energy conservation can also be attributed to a design that places less load on the cooling tower and boiler.

To learn more about how Johnson Controls can help create safe, comfortable and sustainable environments, go to www.johnsoncontrols.com.

About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.

# # #

Share On
Share
Contact
Ryan Nolan
Global Public Relations Program Manager,
Building Technologies & Solutions, Johnson Controls