Johnson Controls announces new Tyco® RFIII Extended Coverage Horizontal Sidewall Sprinkler, rated for light hazard occupancies

Share On
Share

Flat profile design conceals sprinkler in architecturally sensitive installations

MILWAUKEE – (Dec. 6, 2017) – Johnson Controls announces the new Tyco® RFIII Extended Coverage Horizontal Sidewall Sprinkler. This 8.0 K-factor sprinkler is rated for light hazard occupancies and designed to provide protection for coverage areas up to 16 feet by 24 feet (4,9 meters by 7,3 meters) and 18 feet by 22 feet (5,9 meters by 6,7 meters).

The RFIII features a unique flat cover that conceals the sprinkler within the wall, making it an ideal choice for architecturally sensitive installations, such as hotel rooms, reception areas, banquet facilities, conference rooms and hospitals. In addition to a clean look, the sprinkler’s flat profile helps prevent damage and interruption from accidental activations caused by objects being hung from or striking the sprinkler. The cover plate assembly is available in a variety of standard colors, as well as factory-painted custom colors for a seamless, discreet design option.

The push-on closure of the sprinkler allows for ½ inch (12,7 millimeters) of adjustment. The quick response unit also features a sprinkler activation temperature of 160°F (71°C) and a cover plate temperature rating of 139°F (59°C). The sprinkler is UL- and C-UL-listed.

The RFIII joins the Johnson Controls family of Tyco aesthetic sprinklers, which includes RFII flat-plate concealed pendant sprinklers, also available in a range of standard and custom colors, and the Raven Studio sprinkler, available in custom colors or with a paint-in-place escutcheon.

For additional information about the RFIII Extended Coverage Horizontal Sidewall Sprinkler, including the technical data sheet and installation guidelines, visit www.Tyco-Fire.com or contact your local Johnson Controls fire suppression products representative.

About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.

# # #

Share On
Share
Contact
Ryan Nolan
Global Public Relations Program Manager,
Building Technologies & Solutions, Johnson Controls