Multilayer Instrument Cluster

Johnson Controls advances 3D display technology with Multilayer Instrument Cluster concept

Johnson Controls, a global leader in automotive seating, overhead systems, door and instrument panels, and interior electronics, has developed an innovative instrument cluster concept that combines multiple layers of information to generate a three-dimensional (3D) interface. The Multilayer Instrument Cluster concept, which is targeted for full- and mid-size luxury vehicles, creates a more realistic view of the external environment for increased driving efficiency and safety.

“The dynamic movement and interaction of the multiple layers of information offers customers the next-generation of 3D driver assistance,” said Jeff DeBest, vice president and general manager, global electronics for Johnson Controls Automotive Experience. “Our Multilayer Instrument Cluster concept advances the growing trend toward 3D clusters, as its compelling and contemporary 3D graphics showcases the potential of this type of system.”

To address future industry trends and consumer preferences, the Multilayer Instrument Cluster concept employs the latest thin-film transistor (TFT) technology − offering high resolution, brightness and contrast − to create a high-quality 3D interface that’s easy to read. The multi-dimensional visual presents a creative and realistic spatial representation for critical driver information, including speed, navigation and driver assistance systems information. It also allows for the prioritization of information based on driving conditions and can be layered to bring relevant data to the foreground of the cluster and place less important information in the background.

In addition to improved visual appeal, the concept also presents vehicle information directly in front of the driver as opposed to requiring the driver to look elsewhere on the vehicle dashboard. When used with a crash avoidance or driver assistance system, for example, the Multilayer Instrument Cluster offers a highly realistic graphic to demonstrate decreasing distance to a desired exit or the distance between the driver’s vehicle and the vehicle ahead.

A leader in Human Machine Interface technology and development, Johnson Controls is committed to evolving the design and engineering of intuitive technology to enhance driver convenience, usability and safety. The company’s user-centric design approach bridges the cognitive and physical environments to create a seamless and enjoyable user experience, while remaining consistent with vehicle brand and specifications.