Automotive ExperienceVios (1999)
Interiors►
Electronics►
Our Approach►
Featured Stories▼
Leather Wrapping►
ComfortThin Seat►
HomeLink® V►
Concept Cars▼
ie:3 (2011)►
re3 (2009)►
i3 (2007)►
Mesos (2006)►
Ikanos (2005)►
3e (2004)►
Ariston (2001)►
Etimos (2001)►
Kion (2000)►
Vios (1999)►
ESV (1998)►
Symbiosis (1997)►
Natural Materials►
Advanced TPMS►
Open Innovation►
Supplier Information►
The most revolutionary element in the interior of the concept car was the completely redefined instrument panel. All command and control functions were integrated in an exposed center stack and are therefore also easier for the front seat passenger to access. All options corresponded with DIN (German Industrial Norm) measurements, enabling the center stack, as the central element of the instrument panel, to be adjusted to individual requirements.