Johnson Controls/PENN Refrigeration Controls & Controllers

table celltable celltable cell

Stay cool with Johnson Controls/PENN.

From the very beginning, dependability has been a hallmark of Johnson Controls/PENN. We offer proven, long-life durability over a wide range of temperature and pressure applications.

a complete line of high-pressure controls
As part of our ongoing, corporate-wide commitment to sustainability and the environment, we also offer a complete line of high-pressure controls that are compatible with CFC-free R-410A refrigerant. These environmentally-friendly products include the P70 and P170 pressure controls, P100 pressure switches, P266 fan speed controls, and V246 and V248 water regulating valves.

Even though we’ve been around since the beginning of time in refrigeration, Johnson Controls/PENN still delivers the freshest ideas in the business. We’re continuously building on our experience to provide superior control technology for all types of refrigeration and air conditioning equipment. 
 
WHAT'S NEW
Johnson Controls P266 Setup Tool
Check out the new P266 Fan Speed Control Configuration E-Tool
FEATURED BROCHURE
Refrigeration Brochure
We know refrigeration inside and out. 

For 90 years, Johnson Controls/PENN has been the number one choice for refrigeration controls. 
Read More...
Suppliers Employees Contact Site map Privacy Terms of use
© 2012 Johnson Controls. All rights reserved.