Products & Solutions > Building Efficiency > AHR Expo > View from the Show Floor
View from the Show Floor
| January 24, 2008 11:30 am: The Johnson Controls exhibit features a variety of residential Indoor Air Quality solutions, including a hybrid electronic air cleaner, whole home media air cleaners, and large bypass and powered humidifiers. |
|
| NEW YORK -- January 24, 2008 10:00 am: Customers crowd the Johnson Controls booth, learning about new products and applications. |
|
January 23, 2008 4:30 pm: A variable speed drive that features the smallest footprint of any bypass-equipped unit is among a variety of new and innovative products editors are previewing at the Johnson Controls booth. The compact drive has the ability to communicate via BACnet, LonWorks or N2 open protocols and is enhanced with new valves and actuators to provide superior control across a wider range of applications. |
|
| January 23, 2008 1:00 pm: The Johnson Controls booth featured the company’s 7.5-ton rooftop unit. Measuring just 59 inches wide by 89 inches deep, the unit ensures a simple installation, regardless of tonnage. The rooftop unit offers two-stage heat/two stage cooling for ultimate comfort and is charged with environmentally friendly R-410A. |
|
January 23, 2008 11:30 am: The 2007 Reader's Choice Award was presented to Johnson Controls from RSES Journal - for the installation training software for the York Affinity Modulating Gas Furnace. Andy Armstrong, Director of Marketing for Johnson Controls Unitary Products accepted the award from RSES Journal. |
|
|
January 23, 2008 11:30 am: Visitors to booth 1659 got their first look at the new 33-inch York® Latitude™ and Affinity™ furnaces from Johnson Controls. The smaller cabinet makes both the Latitude single-stage furnace and the Affinity modulating gas furnace the compact solution for installations where space is limited. |
|
NEW YORK -- January 23, 2008 10:00 am: Editors investigate new products at the Johnson Controls booth. Over two dozen editors have met with company representatives in the first two days of AHR Expo. |
|
|
January 22, 2008 4:30 pm: Enhancements to the Metasys® building management system from Johnson Controls generated enthusiasm among Expo attendees. The world’s leading building management system now offers a ready access portal that extends usability to operators with fixed tasks and those requiring access from mobile devices. It also supports a large number of simultaneous users and features multiple solutions for data access in both graphical and textual formats. |
| January 22, 2008 2:30 pm: Congratulations to Allan Lee from Baldinger; a Refrigerant Roulette winner! |
|
|
January 22, 2008 1:00 pm: The new York® Tempo™ air-cooled scroll chiller garnered plenty of interest at the Johnson Controls booth. With an integrated part-load value as high as 16.0 EER, Tempo chillers are the most energy efficient in their class. They also offer no ozone depletion and qualify for a LEED® point, making them a smart choice for environment-conscious building owners and designers who are committed to sustainability. |
|
January 22, 2008 11:30 am: Johnson Controls captured the attention of expo attendees with the introduction of a mid-tier offering of air conditioners in the 1.5- to 5-ton range. This new product offering combines the high performance and reliability of York® Latitude™ air conditioners with MicroChannel technology and provides HVAC dealers with a complete selling option to offer homeowners. |
|
|
January 22, 2008 10:00 am: Greetings from the show floor at the AHR Expo at the Javits Center in New York! Johnson Controls will showcase its comprehensive line of commercial and residential HVAC products and systems at booth #1659. |
|
NEW YORK -- January 22, 2008 8:00 am: Johnson Controls has kicked-off AHR EXPO 2008 with a press conference. Several of Johnson Controls’ leaders highlighted the company’s commitments made to creating a more comfortable, safe and sustainable world. Click here for the press release and watch this site for a video of the event. |
|