Building Efficiency Customers and Case Studies
Customers & Case Studies
JOHNSON CONTROLS PROFILED SOLUTIONS:
Digester Gas Cogeneration
Back River Wastewater Treatment Plant, Baltimore, Maryland:
A 3 megawatt combined heat and power plant is expected to generate more than 2.4 megawatts of electricity per year, generate steam to offset process heating requirements and produce hot water for boiler use.
A 3 megawatt combined heat and power plant is expected to generate more than 2.4 megawatts of electricity per year, generate steam to offset process heating requirements and produce hot water for boiler use.
Geothermal
Integrated Design Associates, Inc., San Jose, California:
A heat pump-based HVAC and control system, along with photovoltaics, are key contributors to minimizing the energy consumption in one of the first "net-zero energy" commercial office buildings.
A heat pump-based HVAC and control system, along with photovoltaics, are key contributors to minimizing the energy consumption in one of the first "net-zero energy" commercial office buildings.
Utah Department of Corrections, Utah:
An onsite geothermal well provides heat for multiple buildings and hot water for showers, kitchen and laundry systems. (PDF coming soon.)
An onsite geothermal well provides heat for multiple buildings and hot water for showers, kitchen and laundry systems. (PDF coming soon.)
Landfill Gas To Energy
City of Little Rock, Little Rock, Arkansas:
A methane gas recovery system for the city’s landfill is expected to collect 90,000 MMBTUs of usable energy from landfill gas annually, which will be purchased by an area manufacturer.
A methane gas recovery system for the city’s landfill is expected to collect 90,000 MMBTUs of usable energy from landfill gas annually, which will be purchased by an area manufacturer.
Photovoltaic
29 Palms Marine Base, Palm Springs, California:
We installed a 1.1 MW photovoltaic plant at the Marine Air Ground Task Force Training Command in 29 Palms, CA. This is one of the highest-capacity non-utility solar power plants in the world.
We installed a 1.1 MW photovoltaic plant at the Marine Air Ground Task Force Training Command in 29 Palms, CA. This is one of the highest-capacity non-utility solar power plants in the world.
Solar
City of Tulare, Tulare, California:
We developed a 30-killowatt photovoltaic system on the 20-space carport located at the municipal wastewater treatment plant. It's a great way to showcase the city's commitment to sustainability.
We developed a 30-killowatt photovoltaic system on the 20-space carport located at the municipal wastewater treatment plant. It's a great way to showcase the city's commitment to sustainability.
Wind
Borough of Telford and Wrekin, UK:
A demonstration wind turbine was installed at an elementary school as part of an overall energy management initiative.
A demonstration wind turbine was installed at an elementary school as part of an overall energy management initiative.
City of Geneseo, Geneseo, Illinois:
Construction is nearing completion on two 1.5 MW wind turbines being erected south of the City of Geneseo, in the Quad Cities area of Western Illinois. The turbines will provide up to 30% of the power for the community of 6,400.
Construction is nearing completion on two 1.5 MW wind turbines being erected south of the City of Geneseo, in the Quad Cities area of Western Illinois. The turbines will provide up to 30% of the power for the community of 6,400.
NEW INTERACTIVE RENEWABLES MAP
View our new Interactive Renewables Map...you can review sites where we've done recent renewable energy projects.
Did You Know?
Make sure Javascript is enabled in your web browser, or Click Here to install Flash Player
VIDEO
Wyandotte Public Schools, Wyandotte, Michigan
District teamed with Johnson Controls to reduce operating costs, improve comfort, and implement a solar energy system that doubles
as a learning tool.
District teamed with Johnson Controls to reduce operating costs, improve comfort, and implement a solar energy system that doubles
as a learning tool.