Wind Energy for Main StreetOver the last three decades, the cost of wind energy has dropped dramatically: from over $0.30 / kWh in the mid 1970’s to under $ 0.05 / kWh at today’s best wind sites. Why then don’t we see a wind turbine in the vacant back lot of every school and small business across the windy Midwest? The answer is that, in a few years, you just might. |
|
More and more communities are seeing this “behind the meter” approach as a creative way to directly access the multiple benefits of wind power. Drivers for the rapid expansion of “community wind” include state and federal incentives, increasing costs of carbon based generation, improved low wind speed turbine technology, available means for local long-term project investment, and the increased marketing value of green branding.
The right combination of these factors, or a breakthrough in just one of them, could make wind turbines a common sight on Main Street…or at least in the vacant lot next to Main Street.
Jesse Stowell
Project Development Engineer
Johnson Controls, Inc.