FAQs

Johnson Controls is a Fortune 100 company, with leadership positions in automotive interiors, building efficiency, and power solutions. We are a leading supplier of traditional automotive batteries as well as hybrid battery systems…and also a leader in clean, closed-loop, automotive battery recycling. The company has been instrumental in making automotive batteries the most recycled consumer products in the United States.

Q – What is closed-loop recycling?

A – Johnson Controls uses a closed loop manufacturing and recycling process, which means a used battery never leaves our process from the time it is picked up to the time it is recycled and delivered back to our manufacturing facility to be used in a new battery. The post-consumer lead and polypropylene are reused for battery manufacturing. The electrolyte is transformed into a sodium sulfate salt, which is then used in textiles, glass and detergent manufacturing. And iron byproducts are used in other industrial processes.

Q – Are there any environmental risks associated with the process?

A – No. Lead-acid batteries are the most recycled consumer product in the United States. And Johnson Controls has been a leader in this field. The proposed facility will have state-of-the-art environmental controls, assuring that it conforms well within all federal, state, and local environmental regulations.

More about our Florence facility
Make sure Javascript is enabled in your web browser, or <a href='http://www.adobe.com/products/flashplayer/'>Click Here</a> to install Flash Player
News Feed