Heliar logo
About Heliar
Heliar is the leading Johnson Controls branded battery available in South America, with two production plants based in Sorocaba, Brazil and three distribution facilities in Brazil, Argentina and Venezuela. Heliar batteries are used in automobiles, trucks, and motorcycles. In 2007, Johnson Controls more than 2 million units in the automotive aftermarket, half of which were Heliar brand batteries.

Heliar Solutions
Heliar offers five types of automotive batteries that are specifically designed for different power needs.

  • Heliar Free – Designed for all types of vehicles.
  • Heliar Taxi – Specifically designed for taxis, professional vehicles and vehicles adapted for liquefied natural gas.
  • Heliar Racing – Designed for enthusiastic customers with high power demands, the Heliar Racing battery has the highest reserve capacity, longest life-span and maximum CCA.
  • Heliar Frota – Optimum performance in large trucks, busses and agricultural or industrial vehicles.
  • Heliar Power Sports – Designed to provide optimum performance in motorcycles and other sports vehicles.
Heliar Benefits

  • Help Assistance – Heliar provides consumers with 24-hour roadside assistance in case of electrical failure.
  • Optimal Starting Power – Cutting edge technology allows for maximum CCA.
  • Leak Resistant – Positive and negative grid are expanded to create minimal water loss.
  • Vibration Resistance – 36 percent more weld through the partition allows for better vibration resistance than other batteries.
Heliar Customers
AGCOJohn Deere
AgraleKomatsu
Case New HollandMitsubishi Motors
CaterpillarPSA Peugeot Citroen
Diamler/ChryslerRenault
FiatScania
GMToyota
HondaValtra
Honda MotorcycleVolkswagen
IvecoVolvo

► Download Page as PDF
MEDIA CONTACTS
Power Solutions
Rebecca Fitzgerald
Global Communications Director
414.524.2945
Rebecca_K_Fitzgerald_AT_jci_com 
Suppliers Employees Contact Site map Privacy Terms of use
© 2012 Johnson Controls. All rights reserved.