8 min read
July 01, 2026

Share

Highlights

  • Native server redundancy supports continuous operations without specialized hardware or third-party solutions
  • Built-in cybersecurity features help secure servers and field devices across the system
  • Up to 30% faster engineering and 40% faster upgrades through standardized workflows and pre-emptive system checks, plus up to 80% faster integration than most competitors with visual flow-based programming
  • Up to 30% energy savings through ASHRAE Guideline 36–aligned control strategies
  • An open approach to integration by supporting multiple devices, protocols and systems across portfolios

For more than three decades, building automation has been transforming how facilities operate, adapt and perform. Few platforms have shaped that evolution as consistently or impactfully as Metasys. From early days bringing disparate building systems together to today’s data-rich cyber-resilient environments, Metasys has continuously reflected the principle that buildings are assets that should work for you, bring value to occupants and benefit the bottom line.

Metasys 16.0 takes the next step. It builds on a long legacy of openness, scalability and reliability by responding directly to the demands shaping modern buildings. The latest release is not simply about new functionality; it leads the industry with maximum uptime, internationally recognized cyber resilience and even faster deployment acceleration. It also represents how building automation has become a strategic foundation for sustainability, operational resilience and long-term performance.

“Customers need systems that are resilient by design and simple to deploy and scale. With Metasys 16.0, Johnson Controls brings that together in a single platform.”

- M. Faisal Pandit, President, Building Management Systems, Johnson Controls

Decades in building automation

When Metasys was first introduced in 1990, building systems were largely siloed. HVAC, lighting, fire and security often operated independently, limiting efficiency and visibility. Metasys changed that paradigm by enabling integrated control and monitoring across building systems, which quickly became integral to modern BAS design. Early adoption proved that connecting systems could unlock meaningful gains in reliability, efficiency and occupant comfort.

Over time, Metasys evolved in step with technology shifts. As the industry moved from proprietary hardware toward open protocols and software-driven platforms, Metasys expanded its role. It has evolved from local automation to web-based access, enterprise-scale management and cloud-connected analytics. Each iteration reflects a consistent design philosophy: protecting customer investment while enabling progress.

Shifts in modern building management

Today, building owners and operators face more complex challenges than ever. Rising energy costs, decarbonization goals, cybersecurity risks, regulatory pressure and skilled labor shortages all place greater demands on building automation systems and the facility operators running them. Metasys 16.0 was developed in response to that reality. It shifts focus from managing individual systems to managing outcomes across the building lifecycle.

At the center of this shift is the continued evolution of the Metasys User Interface (MUI). Rather than forcing users to navigate deeply nested system trees, the interface emphasizes workflow efficiency, visualization and context. Equipment, alarms and analytics are tied to the spaces they serve; this allows operators to understand what is happening and why it is important with far fewer clicks.

“The environments our customers operate are more critical than ever, and expectations for performance continue to rise,” said M. Faisal Pandit, President, Building Management Systems, Johnson Controls. “In these environments, even brief disruptions can impact operations, productivity and outcomes. Customers need systems that are resilient by design and simple to deploy and scale. With Metasys 16.0, Johnson Controls brings that together in a single platform. It helps customers maintain continuous operations, reduce risk and adapt as their needs evolve.”

Redundancy as a baseline requirement

As facilities become more connected and mission critical, tolerance for downtime continues to shrink. In environments such as healthcare, laboratories and data centers, even short disruptions can carry operational and financial risks. Metasys 16.0 introduces native, system-level redundancy designed to keep operations running during outages, upgrades and maintenance events.

“With native server redundancy, Johnson Controls combines continuous operator visibility with the ability to act across critical building systems to help ensure resilient, uninterrupted operations,” said Babak Haghayeghi, Product Management Director, BAS, Johnson Controls. “With Metasys 16.0, Johnson Controls delivers real-time visibility into alarms, system status, and critical insights without the need for specialized hardware or third-party solutions. This empowers users to make confident decisions and keep their facilities running seamlessly around the clock.”

By embedding redundancy directly into the platform instead of relying on third-party solutions, Metasys simplifies system architecture while reducing engineering time and costs. Multiple servers can operate in tandem and maintain access to alarms, audits, trends and workflows without interruption. This approach reflects a broader shift in BAS expectations: resilience is not an optional add-on; it’s a design requirement.

Safeguarding facilities and exceeding demanding regulatory requirements

Metasys uses zero trust technology, encrypted communication and cybersecurity best practices – including password and account management – to meet even the most stringent regulatory and certification requirements.

Key features include:

  • The award-winning Cyber Health Dashboard, highlighting potential security concerns
  • Multiple secure methods for connectivity, including IEEE802.1x support and BACnet/SC
  • IEC62443-4-2 SL2 compliance, laying the groundwork for EU Cybersecurity Resilience Act readiness by 2027 – including authentication, encryption, integrity checks and secure communications
  • Advanced user permissions to streamline system administration

With enhanced cybersecurity built into every layer, Metasys 16.0’s zero trust architecture, encrypted communications and adherence to industry best practices work together to safeguard your building systems while simplifying compliance.

“With native server redundancy, Johnson Controls combines continuous operator visibility with the ability to act across critical building systems to help ensure resilient, uninterrupted operations.”

- Babak Haghayeghi, Product Management Director, BAS, Johnson Controls

Turning building data into swifter decisions

Data has always been central to building operations, but its value depends on context and accessibility. Metasys 16.0 expands native energy management and reporting capabilities, making it easier to translate raw data into actionable insight. With three-click dashboard configuration, users can easily visualize energy consumption, cost, demand and emissions without relying on external analytics platforms.

These capabilities support energy optimization, compliance with evolving regulations and sustainability-reporting requirements. Metasys 16.0 is also compliant with automated energy performance reporting; it generates energy reports aligned with EPBD and US standards, supports audits, simplifies benchmarking and enables compliance. (e.g. LL97, Title 24, BERDO).

Integrated dashboards and reports provide consistent, auditable data from a single source of truth. This can help reduce manual efforts at a time when experienced workers are retiring and replacement hires are difficult to find.

Metasys 16.0: Open by design

Metasys takes an open approach to integration by supporting multiple devices, protocols and systems across portfolios. Metasys 16.0 offers enhancements supporting AI-based integration and low-code connectivity options. With security built into every layer, and alignment with IEC 62443-4-2 Security Level 2, users stay ahead of risk and regulatory demands.

The result? A platform that evolves with technology strategies, rather than constraining them.

As buildings increasingly connect to enterprise systems, analytics platforms and AI-driven services, openness becomes a competitive advantage. Metasys 16.0 provides a flexible foundation that allows organizations to innovate at their own pace, while maintaining control of core operations.

Request a personalized demo

Request demo

Metasys today:

  • Over 54,000 installations worldwide
  • Energy monitoring, made simple
    • A typical 100,000 sq ft building spends $300k annually on energy. Insights gained from the Energy Management suite can translate to savings ranging from $7.5k - $30k per year
    • ASHRAE Guideline 36 standardized HVAC control sequences are built in for both airside and waterside applications. Speed engineering and implementation, maximize HVAC system performance and cut energy use up to 30%
  • Up to $37K savings and 40 hours reduced engineering effort per site
  • Fault Detection and Triage can reduce cost to diagnosis by 50% - identifying and managing equipment that isn’t operating properly and guiding staff on how to quickly address issues
  • Up to 95% faster upgrades with Metasys Fast Track Upgrade

A platform shaped by experience

More than 30 years after its introduction, Metasys remains central to the Johnson Controls vision for smarter, safer, sustainable facilities. Metasys 16.0 does not replace that legacy – it builds on it by applying decades of real-world experience to the challenges building owners and operators face today.

From resilience and cybersecurity to energy intelligence and usability, Metasys 16.0 reflects a clear understanding of what matters most to operators and owners. It’s a platform designed for what buildings are and what they are becoming. Johnson Controls will be there every step of the way.

Contact Johnson Controls to request a Metasys 16.0 demo today

Contact us

FAQs

What makes Metasys 16.0 different from previous versions?

Metasys 16.0 focuses on platform-level innovation by embedding native redundancy and built-in cybersecurity at every layer. It delivers 40% faster upgrades, reduces complexity and increases long-term value.

How does Metasys 16.0 support sustainability and compliance goals?

The platform includes native energy monitoring, emissions visibility and reporting capabilities. These features help organizations track performance, validate savings and align with evolving regulatory requirements.

Is Metasys 16.0 only intended for new construction projects?

No. Metasys 16.0 includes tools that streamline upgrades and modernization. This allows existing customers to preserve past investments while gaining access to new capabilities and improved performance.