- Johnson Controls
- Customer Success Stories
- Ivy League Library Protection
Protecting Priceless Pages with Sustainable Fire Suppression
With ANSUL® INERGEN® technology, the library gained more than a fire suppression system—it gained a sustainable protection strategy for safeguarding history. By combining clean agent performance, design flexibility, occupant safety, and long-term environmental assurance, Johnson Controls helped ensure that these rare materials can continue to inform, inspire, and endure for generations to come.
Impact Highlights
Sustainable protection: Uses naturally occurring atmospheric gases to help reduce environmental impact while providing effective fire suppression.
Collection- and people-safe: Leaves no residue, avoids water damage, and is non-hazardous for employees, researchers, students, and visitors.
Flexible, long-term assurance: Supports remote cylinder placement and is backed by 20-Year Environmental and Evergreen Discharge Warranties.
Protect priceless rare books and manuscripts without risking damage from conventional fire suppression methods
The Ivy League Rare Book and Manuscript Library in New Haven, Connecticut, houses hundreds of thousands of rare books and several million manuscripts, including a Gutenberg Bible and works by Charles Dickens and Benjamin Franklin. Protecting these irreplaceable collections from fire was critical, but traditional suppression methods posed a significant risk. Water and other conventional agents could cause extensive damage to rare books, manuscripts, and archival materials. Additionally, the library required a solution that could accommodate unique architectural constraints while providing long-term protection for both the collection and occupants.
ANSUL® INERGEN® Clean Agent Fire Suppression System
The library selected the ANSUL® INERGEN® Clean Agent Fire Suppression System, a sustainable fire protection solution that delivers effective suppression without compromising valuable assets or the environment. Composed of naturally occurring atmospheric gases, INERGEN® provides fire suppression without leaving residue, damaging sensitive materials, or creating environmental concerns associated with some alternative agents.
The system addressed several key challenges:
- A gentle discharge protected delicate books and manuscripts, with testing confirming that not a single sheet of paper was displaced.
- The agent maintained the required design concentration beyond the NFPA 2001 minimum requirement, ensuring effective fire suppression.
- Long-distance agent flow enabled remote cylinder placement, providing greater flexibility within the library's unique structure.
- Because INERGEN® is made from gases already present in the atmosphere, it offered an environmentally responsible solution that protects people, property, and valuable collections.
Sustainable, environmentally responsible fire protection that safeguards rare collections, building occupants, and the environment
The ANSUL® INERGEN® system delivers comprehensive protection for one of the world's most important, rare book and manuscript collections while supporting the library's commitment to preserving resources for future generations. The environmentally friendly, non-hazardous agent safeguards priceless historical materials without exposing them to water damage or harmful residues. At the same time, it provides a people-safe solution for employees, researchers, and visitors occupying space.
By choosing INERGEN®, the library gained a fire suppression solution that protects irreplaceable cultural assets while minimizing environmental impact.
Similar stories
San Francisco International Airport strengthens fire protection and operational continuity with advanced foam suppression system
SFO partnered with Johnson Controls to implement a high-performance, non-fluorinated foam suppression system that delivers fast, reliable fire protection while supporting long-term operational resilience.
Protecting over 600,000 artifacts at Mexico City’s National Museum of Anthropology
Advanced fire detection and clean-agent suppression systems safeguard one of Latin America’s most important cultural collections while supporting safety and compliance.
Custom Fire Protection Solutions Deliver Significant Economic and Operational Benefits
Johnson Controls partners with a global retailer to upgrade fire protection systems across thousands of stores with minimal operational disruption
Fire Protection for Frasers Group’s Automated Warehouse
Frasers Group implemented a bespoke fire detection and extinguishment system to safeguard its 13,000 m² automated warehouse and maintain operational continuity.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)