Integrated controls support changing exhibition schedules and large-scale events

The development is one of the largest exhibition and trade complexes in central China. The 527,000-square-meter, multi-venue complex includes 13 standard exhibition halls, three multifunctional halls, and supporting commercial and operational facilities. With approximately 15,000 building management system control points, the project needed to integrate multiple building systems while responding to changing exhibition and event schedules. EasyIO controls enabled centralized, schedule-driven management, zone-based operation and precise equipment control, reducing commissioning time, energy consumption and on-site workload.

Impact Highlights

Up to 20% less commissioning time

Sustainability

Up to 15% lower energy consumption

15% less on-site workload

Integrating complex venue systems within a compressed project timeline

The development needed to integrate multiple building systems across a large, complex venue. Its 16 exhibition halls and supporting commercial and operational facilities created a multi-venue environment with approximately 15,000 building management system control points.

Operations also had to respond to changing exhibition and event schedules. The project needed to maintain comfort and efficiency as demand shifted between daily operations and large-scale events, while coordinating HVAC, ventilation and energy systems throughout the complex.

The integrated system also had to be delivered and optimized within a compressed project timeline. This required an approach that could support efficient, reliable performance across the development while simplifying the work required on site. The project therefore needed controls that could manage a large number of points, integrate essential systems and adjust equipment operation to the demands of each exhibition zone.

Centralized, zone-based control aligns operation with venue demand

The project deployed 507 EasyIO Neo Series CW IP controllers and nearly 2,000 I/O modules across the 527,000-square-meter development. The controls support the complex’s approximately 15,000 building management system control points.

Centralized, schedule-driven building control enables the facility to coordinate operations across its exhibition halls and supporting spaces. Zone-based control aligns equipment operation with exhibition demand as schedules and venue requirements change.

The project also uses precise temperature and equipment control to optimize comfort and energy performance. This approach supports both daily operations and large-scale events across the complex’s 13 standard exhibition halls, three multifunctional halls, and supporting commercial and operational facilities.

An integrated building management approach brings HVAC, ventilation and energy systems together. EasyIO Neo Series CW IP controllers, an EasyIO 8000 network controller and I/O modules provide the control infrastructure for efficient, reliable performance across the multi-venue environment. By combining centralized scheduling with zone-level control, the solution addresses both the scale of the development and the changing operational requirements of exhibitions and events.

Measurable reductions in commissioning time, energy use and site workload

Automated optimization reduced commissioning time by up to 20%, helping the project deliver and optimize the integrated system within its compressed timeline. The deployment also reduced on-site workload by 15%.

Precise control reduced energy consumption by up to 15%. Centralized scheduling and zone-based control align equipment operation with exhibition demand, supporting daily operations as well as large-scale events.

The integrated approach brings HVAC, ventilation and energy systems together across approximately 15,000 building management system control points. The source reports that more stable operation supports longer equipment life and reduced maintenance.

Across the complex, centralized and schedule-driven control simplifies operations, while zone-based control aligns equipment use with exhibition demand. Precise temperature and equipment control supports comfort and energy performance as the venue moves between daily operations and large-scale events. Together, these outcomes support efficient, reliable performance across the large, multi-venue environment.

About the Customer

The customer operates one of the largest exhibition and trade developments in central China. The 527,000-square-meter, multi-venue complex includes 13 standard exhibition halls, three multifunctional halls, and supporting commercial and operational facilities for daily operations and large-scale events.

Building Insights

The one-stop shop for smart buildings news and insights

Take a look

About the facility

  • 527,000-square-meter exhibition and trade development in central China
  • 13 standard exhibition halls and three multifunctional halls
  • Approximately 15,000 building management system control points

Solutions:

Share

Similar stories

Building

Graha CIMB Niaga improves energy efficiency in Jakarta

Across its 30,000 m² tower, Graha CIMB Niaga achieves measurable energy savings. With Metasys centralizing HVAC control, the officer tower boosts transparency and streamlines daily operations.

Thamrin Nine

Thamrin Nine delivers up to 30% energy savings

Thamrin Nine achieved Green Mark Platinum certification with YORK chillers and Metasys, delivering up to 30% energy savings and high-efficiency cooling performance.

Global Consulting Company

Global consulting firm sees 17% energy savings and reduces CO2 emissions

Company realizes significant financial impact while improving air quality, occupancy comfort and productivity.

Building picture

The Wings sets a new efficiency standard in Europe

The Wings in Belgium delivers triple-certified sustainable performance across its 50,000 m² mixed-use campus. With Metasys unifying HVAC and energy systems, the site cuts energy use, lowers emissions and streamlines daily operations through data-driven building automation.

Contact us

Please read our Privacy Notice for information on how we protect and manage your personal data. By completing this form and submitting your information, you confirm that you have reviewed, understood and accepted our privacy terms as well as our cookie terms.