- Johnson Controls
- Customer Success Stories
- Torre Mayor
Advancing energy efficiency and sustainability at Torre Mayor through HVAC and BAS upgrades
Modernizing an iconic building to support long-term sustainability
Impact Highlights
10% energy cost savings
40–45% energy savings during partial load conditions
Improved temperature comfort for occupants
Upgrading critical building systems without disrupting operations
After more than 20 years of operation, Torre Mayor set out to modernize its HVAC and building automation systems to maintain high performance, improve energy efficiency, and support its sustainability objectives, including LEED certification.
As one of Mexico City’s most prominent office towers, the building required solutions that could extend system life while meeting evolving efficiency standards. The project involved integrating energy-efficient, low-GWP HVAC equipment within existing infrastructure constraints, including fixed dimensions, connections, and water intakes.
Limited access and tight installation spaces added complexity. At the same time, Torre Mayor required greater visibility and control across building systems through an upgraded automation platform. All work had to be completed while the building remained fully operational, without disrupting occupants or daily business activities.
Integrated HVAC and building automation modernization
To address these challenges, Torre Mayor worked closely with Johnson Controls to design an integrated solution that balanced energy performance, operational continuity, and long-term sustainability. The approach focused on upgrading core building systems while adapting to existing conditions and minimizing disruption.
The solution included a 900 TR YORK® centrifugal chiller, designed for high efficiency during partial load conditions, using a low-GWP refrigerant to support sustainability and LEED requirements, and engineered to meet the building’s physical constraints.
In parallel, Torre Mayor upgraded to the latest version of the Metasys Building Automation System, enabling centralized monitoring and control of more than 6,000 points across critical building systems, including HVAC, access control, and fire detection and suppression.
Together, these upgrades improved system integration and supported more informed, data-driven decision-making, laying the foundation for improved energy efficiency and long-term building performance.
“Johnson Controls not only boasts a reputation earned through daily dedication, but also utilizes state-of-the-art equipment and is always looking for ways to improve.”
Felipe Flores
Chief Operating Officer, Torre Mayor
Improved efficiency, comfort, and long-term sustainability
As a result of the HVAC and building automation upgrades, Torre Mayor reduced energy costs, improved indoor comfort, and strengthened the efficient management of building resources through management and monitoring systems. The project also supported increased productivity while maintaining uninterrupted building operations.
Key outcomes include:
- Achieved 10% energy cost savings
- Up to 45% HVAC energy savings during partial load conditions
- Improved temperature control and occupant comfort
- Optimized building operations through integrated automation
- Completed the upgrade with zero operational disruption
About Torre Mayor
About the facility
- Paseo de la Reforma, Mexico City, Mexico
- 84,135 m² office tower, 59 floors
- Over 8,000 occupants
Solutions:
Similar stories
Graha CIMB Niaga improves energy efficiency in Jakarta
Across its 30,000 m² tower, Graha CIMB Niaga achieves measurable energy savings. With Metasys centralizing HVAC control, the officer tower boosts transparency and streamlines daily operations.
Global consulting firm sees 17% energy savings and reduces CO2 emissions
Company realizes significant financial impact while improving air quality, occupancy comfort and productivity.
The Wings sets a new efficiency standard in Europe
The Wings in Belgium delivers triple-certified sustainable performance across its 50,000 m² mixed-use campus. With Metasys unifying HVAC and energy systems, the site cuts energy use, lowers emissions and streamlines daily operations through data-driven building automation.
Dubai Silicon Oasis achieves 30% annual energy savings with AI‑powered solutions
Energy‑efficient strategies and data‑driven services help Dubai Silicon Oasis achieve measurable energy savings and carbon‑reduction impact.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)