- Johnson Controls
- Customer Success Stories
- University Stadium
University stadium prioritizes occupant safety with upgraded fire and emergency communications systems
Upgraded fire and emergency communications systems support stadium safety and operations
Impact Highlights
Improved visibility to identify and respond to incidents across the stadium
Reduced incident response times through integrated emergency communications
Integrated systems to pinpoint the source of fire and emergency events
Ensuring occupant safety and operational control in a high-capacity stadium
At large universities, stadium operations teams are responsible for the safety of thousands of occupants during high-attendance events. With a capacity of over 80,000 people, the university needed to mitigate risk and ensure occupant safety while maintaining seamless game day operations.
Following a major renovation, university leaders took the opportunity to implement a long-overdue upgrade to the stadium's fire and emergency communications technology.
Integrated fire detection and emergency communication systems for full stadium coverage
Johnson Controls worked with the university's fire department and local Fire Marshal to evaluate existing systems and develop a coordinated upgrade plan. The team collaborated with university stakeholders to design and implement system upgrades, holding recurring meetings to ensure alignment and progress.
To meet project timelines and deliver upgrades across the stadium, additional subcontractors were engaged to support electrical work. Through the installation of fire panels and addressable strobe technology, stadium personnel can identify incidents and deploy on-the-ground teams more effectively.
Enhanced incident visibility and faster response across the stadium
With upgraded fire and emergency communication systems in place, stadium operations and security personnel can quickly identify and respond to incidents.
Outcomes include:
- Improved visibility into fire and emergency events throughout the stadium
- Reduced incident response times through integrated emergency communications
- Enabled faster deployment of on-the-ground personnel
- Supported targeted evacuations during emergency situations
About the University Stadium
About the facility
- Large university stadium
- Capacity of over 80,000 occupants
Solutions:
Similar stories
Fire Protection for Frasers Group’s Automated Warehouse
Frasers Group implemented a bespoke fire detection and extinguishment system to safeguard its 13,000 m² automated warehouse and maintain operational continuity.
Protecting over 600,000 artifacts at Mexico City’s National Museum of Anthropology
Advanced fire detection and clean-agent suppression systems safeguard one of Latin America’s most important cultural collections while supporting safety and compliance
Supporting fire safety in a critical defense manufacturing environment
A leading Indian defense and aerospace manufacturer required advanced fire protection and detection systems for a large-caliber ammunition manufacturing complex in Kanpur.
Custom Fire Protection Solutions Deliver Significant Economic and Operational Benefits
Johnson Controls partners with a global retailer to upgrade fire protection systems across thousands of stores with minimal operational disruption

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)