Tyco Security Products introduces Kantech EntraPass access control system onboard exacqVision network video recorders

Share On
Share

exacqVision Recorders with access control pre-licensed simplifies installation and saves money

 

access control onboard

WESTFORD, MA. February 9, 2016 — Tyco Security Products introduces exacqVision network video recorders (NVR) with Kantech EntraPass Corporate Edition access control system pre-installed for faster, simpler security installation and service.

exacqVision NVRs provide high performance, all-in-one network video surveillance solutions. Available in hybrid and IP camera NVR models, exacqVision recorders deliver reliability and capacity for mainstream recording.

Designed for easy installation, Kantech EntraPass Corporate Edition comes pre-installed and pre-licensed on exacqVision A-Series and Z-Series Windows NVRs. Having the access control system loaded onto the video server saves users hardware, power and cooling costs while also reducing the amount of rack space required.

Users can control a handful of doors or millions from multiple locations worldwide. Each recorder will support up to 20 workstations and up to 50 concurrent instances of EntraPass Web or EntraPass Go mobile application.

Live and recorded video can be viewed and managed directly from the recorder using the included exacqVision client or remotely using a web browser or exacqVision client on a separate computer. The freely distributed client software can be installed on Windows, Linux or Mac systems. exacqVision CameraLinks puts the most needed access control commands at the operator’s fingertips in the live video view. Using CameraLinks, users can configure overlay controls that will display when hovering over a camera in live view for quicker response to critical alarms and events.

“Adding Kantech EntraPass access control system onto our exacqVision recorders enables our users to manage and configure both video and access control from a single interface for a more cost-effective, complete security solution,” said Scott Dennison, Director of Marketing, Exacq Technologies. “Combining access control on our recorder product also simplifies deployment for installers, saving both time and money.”

For a complete security solution, users have the ability to easily integrate DSC PowerSeries Neo intrusion devices. Combining live and recorded video with access control and intrusion detection events unifies security functions as an all-in-one solution, reducing duplicate efforts.

Each exacqVision recorder includes a three-year hardware warranty and three years of free software updates.

For more information on this exacqVision recorder and other new offerings, go to www.exacq.com.

- End -

About Exacq
Exacq Technologies is part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Exacq Technologies (
www.exacq.com) designs and manufactures the cross-platform, open-architecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-platform (Windows/Linux/Mac) client, most web browsers and via the free Exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world via authorized resellers and distributors.

About Kantech
Kantech access control solutions are part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Kantech access control technologies are ready to use right out of the box, and provide solutions that are compact, and easy to use for smaller businesses while scaling to meet the needs of larger businesses. Kantech solutions can easily link to American Dynamics video systems and DSC alarm panels to provide an integrated, holistic security solution. To learn more about Kantech products, visit 
www.kantech.com


About Tyco Security Products
Tyco Security Products and its leading brands conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences. 

Share On
Share