ExacqVision 7.6 improves client performance

Share On
Share

exacqVision 7.6 also includes new area zoom, enhanced searching in Exacq Mobile, new IP camera integrations and more

INDIANAPOLIS — With the release of exacqVision 7.6 video management system (VMS) software, Tyco Security Products increases local client video performance on all exacqVision network video recorders (NVR) and client workstations. exacqVision version 7.6 video management system (VMS) software also includes new area zoom, mapping functionality, faster searching in Exacq mobile and automatic updates across all exacqVision software in Enterprise System Manager (ESM), a health monitoring program for use with exacqVision Enterprise network video recorders (NVRs).

With exacqVision version 7.6, the exacqVision client has increased local client video performance for all exacqVision recorders and client workstations that have discrete or integrated graphics processors. In large installations with many cameras, operators can achieve a higher frame rate on more cameras when monitoring in live view.

In live view, users can utilize a new pan-tilt-zoom (PTZ) functionality, area zoom. This allows a box to be drawn around a specific region in live view to instantly optically zoom in to see greater detail on objects or people in the distance. Area zoom is available for Axis and Illustra PTZ cameras used with exacqVision.

The 7.6 release introduces field of view indicators on exacqVision maps.exacqVision Professional and Enterprise users can add new indicators to visualize the camera coverage in the environment. Users also have the ability to change the color of the field of view indicators to more easily identify particular regions on the map. Further, to simplify mapping users can drag and drop maps and child maps anywhere in the tree to organize into hierarchical nesting for faster navigation.

For European customers, exacqVision presents the ability to configure enhanced privacy restrictions requiring a second reviewer to view live video or review recorded video.

The latest version of Exacq Mobile app for iOS, Android and Windows Phone 8 devices improves search capabilities. Through the Exacq Mobile app, within one click users can quickly pick a pre-defined search range from five seconds to 15 minutes to immediately see search results for the camera in the current view. Additionally, new time controls have been introduced for custom time searches.

Enterprise System Manager (ESM) offers administrators more tools to perform software updates. With the improved available versions page, ESM provides quick identification of the current versions installed across the environment. Administrators will receive notifications when newer versions are available and can update all exacqVision client and web services directly from ESM.

exacqVision VMS now supports nearly 3,000 IP camera models including the new Illustra Pro 2MP mini-dome cameras featuring UltraVision low light technology.

The exacqVision VMS is accessed with the freely distributed exacqVision client software (Windows/Linux/Mac), the exacqVision free web browser client available for all leading web browsers (Google Chrome, Firefox, Internet Explorer, Safari and Opera), as well as the free Exacq mobile app for iOS, Android and Windows Phone 8 devices. The VMS software is included with pre-configured exacqVision NVR servers or it can be installed on third-party Windows or Linux-based systems.

For more information on this exacqVision software release and other new updates and offerings, go to www.exacq.com.

# # #

About Exacq

Exacq Technologies is part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Exacq Technologies (www.exacq.com) designs and manufactures the cross-platform, openarchitecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-platform (Windows/Linux/Mac) client, most web browsers and via the free Exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world via authorized resellers and distributors.

About Tyco Security Products

Tyco Security Products and its leading brands conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential. Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.

MEDIA CONTACT

Andrea Gural / Chelsie Woods

Eclipse Media Group

+1 207-319-7372 / +1 207-510-0029

agural@eclipsemediagroup.net

cwoods@eclipsemediagroup.net

Share On
Share