Tyco Security Products debuts integrated SALTO lock solution for access control

Share On
Share

salto offline lock1 p3 WESTFORD, MA. – April 6, 2016 –– Tyco Security Products announces the integration of its C•CURE 9000 security and event management system from Software House with SALTO offline locks for seamless access control of an entire building through a single user interface. The integration between Salto and Software House will be on display at the Tyco Security Products booth 20005, at ISC West, April 6-8, in Las Vegas, Nev.

The C•CURE 9000/SALTO solution is ideal for access control systems that require varying levels of security for interior and exterior access points. The solution deploys SALTO offline locks for interior doors that require a moderate level of security, such as storage and office areas, while Software House hard-wired door controllers are used for high security and perimeter access points. With this solution, security operators can control access to all doors into and within the facility through the C•CURE 9000 user interface, based on communications between C•CURE 9000 and the SALTO server.

“The C•CURE 9000/SALTO solution is a powerful integration that simplifies access control management by joining offline locks and hard wired doors together,” said Jason Ouellette, Product Line Director, Access Control, Tyco Security Products. “With C•CURE 9000 and SALTO, facilities can manage their entire access control infrastructure with a single credential and management platform.”

The C•CURE 9000/SALTO solution supports a nearly unlimited number of offline locks and uses SALTO online readers to update cards for offline reader access. The use of access cards for doors instead of mechanical keys results in cost savings, saving human and monetary resources previously spent on lost key replacement. The C•CURE 9000 guided user interface and single sign-on credentialing makes access control management more efficient and user-friendly.  With the C•CURE 9000/ SALTO lock solution, no cabling is required for lock installation and offline locks can be installed on almost any door type.

For more information on Software House’s C•CURE 9000/SALTO solution, visit Software House at www.swhouse.com, or visit Tyco Security Products’ booth at ISC West 2016, booth 20005.

- End -

About Software House 
Software House security and event management systems are part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Software House’s innovative C•CURE software portfolio combines with a suite of reliable controllers to provide the most powerful security and event management in the industry. Add an unsurpassed integration platform that allows customers to integrate seamlessly with critical business applications, and it’s easy to see why Software House solutions are ideal for security-critical applications. For more information about Software House products, visit 
www.swhouse.com.

 

About Tyco Security Products
Tyco Security Products and its leading brands conduct business in over 177 countries around the world, in multiple languages and employ over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities and over five million private residences. 

Share On
Share