Tyco Security Products offers EyeLock nano NXT® Iris authentication technology for access control

Share On
Share

The advanced biometric identifier integrates with Software House’s C•CURE 9000 security and event management platform

EyeLock nano NXWESTFORD, MA. June 30, 2016 –– Tyco Security Products introduces the integration of EyeLock nano NXT® advanced dual iris authentication technology with Software House’s C•CURE 9000 security and event management solution.

An ideal solution for business, government and other applications, EyeLock nano NXT uses video, rather than still pictures, to capture eye images at 20 frames per second. EyeLock’s technology converts the unique characteristics of each iris into encrypted code, creating a high level of security with a false accept rate during authentication of 1 in 1.5 million for a single eye. The biometric identifier can authenticate up to 20 people per minute while in-motion and at-a-distance of 12 inches.

“Tyco Security Products continues to build its biometric integration portfolio, offering customers the latest and most accurate technologies available,” said Jason Ouellette, Product Line Director, Access Control, Tyco Security Products. “The availability of EyeLock nano NXT for use with C•CURE 9000 presents end users with expanded options for a highly secure access control solution.”

The EyeLock nano NXT can be deployed within a networked C•CURE 9000 platform and can serve as part of a two-factor authentication process. The compact EyeLock nano NXT, which measures just 8 inches by 5 inches, offers an on-board memory of up to 20,000 unique users.

Additional features of EyeLock nano NXT include tamper detection and a web configuration tool. Customization is available through an optional SDK.

For more information, visit Software House at www.swhouse.com.


- End -

 

About Software House 
Software House security and event management systems are part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Software House’s innovative C•CURE software portfolio combines with a suite of reliable controllers to provide the most powerful security and event management in the industry. Add an unsurpassed integration platform that allows customers to integrate seamlessly with critical business applications, and it’s easy to see why Software House solutions are ideal for security-critical applications. For more information about Software House products, visit 
www.swhouse.com


About Tyco Security Products

Tyco Security Products is a unified group of the most comprehensive world-leading premium access control, video, location-based tracking and intrusion solutions in the security industry. Tyco Security Products conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.

Share On
Share