Minnesota casino migrates to IP video surveillance with victor from Tyco Security Products

Share On
Share

The American Dynamics’ video management platform provides the versatility and high image quality needed for one of the state’s most popular casino destinations

Fond Du Luth ExteriorWESTFORD, MA — July 28, 2016 – Tyco Security Products has announced that Fond-du-Luth Casino in Duluth, Minn., has selected its victor video management system as the core platform for its new fully-IP-based video surveillance system, which includes hundreds of new Illustra IP cameras and several new VideoEdge network video recorders (NVRs). With victor at the center of its new system, the casino is able to streamline its surveillance operations, drastically improve video image quality and monitor live and recorded video faster.

With the help of its systems integration firm, Brick, N.J.-based North American Video, Fond-du-Luth Casino chose American Dynamics’ victor as its new IP-based video management system because of its intuitive and powerful user interface that allows the casino to view and manage all of its video through a single user GUI interface or a Matrix switcher keyboard. Fond-du-Luth’s surveillance operators can quickly identify security issues using victor’s Command Center feature with its Virtual Matrix, which lets operators view live and recorded video, select cameras and communicate quickly between security operator workstations. Fond-du-Luth’s surveillance operators use American Dynamics’ 2089 matrix keyboards to search video history in a matter of seconds and search across multiple recorders simultaneously when performing investigations.

Illustra Pro IP PTZ cameras give the casino the high-resolution video quality necessary for monitoring live and recorded activity. The cameras’ fast positioning speed, up to 512° per second, allows surveillance officers to quickly identify suspicious activity at distances of up to 1,000 feet from an individual camera.

“The efficiency and speed of the Illustra cameras plus the comprehensive view that victor gives us is exactly what we were looking for in our migration to IP-based video surveillance,” said Dennis McCauley, Fond-du-Lac’s Lead Surveillance Technician. “When you add to that the versatility of VideoEdge, our surveillance officers have more time to devote to active surveillance because they know that they can depend on the new system to take care of everything else.”

The Fond-du-Luth Casino is owned and operated by the Fond du Lac Band of Lake Superior Chippewa of Minnesota. The Band is currently working with systems integrator NAV to add additional cameras to the casino and plans to expand the casino’s footprint and to integrate its access control system with victor in the near future.

- End -

About Tyco Security Products
Tyco Security Products is a unified group of the most comprehensive world-leading premium access control, video, location-based tracking and intrusion solutions in the security industry. Tyco Security Products conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.

Share On
Share