Tyco announces new listing for ESFR-25 pendent sprinklers for warehouse and storage applications

Share On
Share

Model ESFR-25 (TY9226) protects higher at narrower aisle widths

LANSDALE, PA. (August 2, 2016) –– Tyco Fire Protection Products (TYCO), a global leader in fire suppression technologies, announces the TYCO Model ESFR-25 Early Suppression Fast Response (ESFR) Pendent Sprinkler (TY9226) with a K-Factor of 25.2 for warehouse and other storage applications. The sprinkler provides an industry first 48 feet ceiling height protection with a minimum five-foot aisle width.

The new listing for the ESFR sprinkler provides more installation flexibility, as no other sprinkler can match the performance at that height with such a narrow aisle width. The Model ESFR-25 Pendent Sprinkler is listed and approved for a wide range of storage arrangements and commodity classing, including the most common storage materials, encapsulated and nonencapsulated class I-IV commodities and expanded and unexpanded plastics.

The new Model ESFR-25 sprinkler is UL and C-UL Listed for ceilings up to 48 feet (14,6 m) high and storage heights up to 43 feet (13,1 m) and fully complies with UL 1767 new Section 30A – high clearance fire test and is FM approved for installation according to FM Global Loss Prevention Data Sheets. The sprinkler is available with either NPT or ISO threads and with ordinary and intermediate temperature ratings of 165°F (74°C) and 212°F (101°C) respectively.

Contact Tyco Technical Services for the latest approval information. For additional information on the new Model ESFR-25 sprinkler, see datasheet TFP312, at www.tyco-fire.com

About Tyco Fire Protection Products

Tyco Fire Protection Products is a division of Tyco, the world’s largest pure-play fire protection and security company. As an industry leader, Tyco Fire Protection Products uses its global scale and deep expertise to drive innovation, advance safety and solve the unique challenges of customers in more than 190 countries worldwide. Every day, Tyco Fire Protection Products manufactures and delivers an unmatched range of detection and suppression systems, extinguishing agents, sprinkler systems, valves, piping products, fittings, fire-fighting equipment and services that can help its customers save lives and protect property. Its global technology portfolio includes fire suppression, fire detection and mechanical building product offerings sold under many of the world's best-known brands: ANSUL, CHEMGUARD, EZCARE, FIRECLASS, FLAMEVISION, GRINNELL, HYGOOD, LPG, NEURUPPIN, PYRO-CHEM, RAPID RESPONSE, SABOFOAM, SHURJOINT, SIMPLEX, SKUM, SPRINKCAD, THORN SECURITY, VIGILANT, WILLIAMS FIRE & HAZARD CONTROL, and ZETTLER. For more information, visit www.Tycofsbp.com. 

 

Contacts:

Krista Hazen

SBC Advertising

614.255.2333

khazen@influencesbc.com

Share On
Share