ExacqVision 8.0 introduces suspect tracking

Share On
Share

exacqVision 8.0 also includes new archive bookmarks, IP camera integrations and more

exacqVision 8-0_exacqReplay

INDIANAPOLIS, September 15, 2016  — With the release of exacqVision 8.0 video management system (VMS) software, Tyco Security Products introduces suspect tracking, a new way to follow a person or object of interest through the entire scene. exacqVision version 8.0 video management system (VMS) software also includes new archiving for bookmarked video, activity timeout and camera inspection in Enterprise System Manager (ESM), a health monitoring program for use with exacqVision Enterprise network video recorders (NVRs).

With the new suspect tracking feature in exacqVision version 8.0, users can track suspects through multiple camera views by drawing a transparent box in a specific area and linking that to other adjacent cameras with CameraLinks. Through exacqVision search tools, users can also create a suspect tracking search. In addition to suspect tracking, operators can access exacqReplay directly from live view with CameraLinks for an instant replay of video and audio.

Bookmarked video can be archived separately from other footage to create a second copy of important video. In retail applications, a corporate security officer can bookmark video of an incident at a specific store and then archive it automatically to the corporate network share overnight during off peak hours. Afterwards, exacqVision users can directly search bookmarks on the archive while not limiting WAN bandwidth.

exacqVision 8-0_Suspect_tracking

To further conserve bandwidth, exacqVision will now blank video panels when the client has been inactive for a designated amount of time. exacqVision 8.0 also allows users to configure the color and background of serial data displayed in live view to easily read associated data such as license plates and receipt transactions.

Enterprise System Manager (ESM) offers camera inspection. With the web service deployed, administrators can visually compare camera views to reference images and identify and denote cameras needing adjustment. Additionally, ESM users can generate camera assessment reports to be used by technicians on site to simplify camera inspection services.

exacqVision VMS now supports more than 3,000 IP camera models including cameras from Illustra, Axis Communications, Arecont Vision, Panasonic and other leading IP camera manufacturers. exacqVision 8.0 adds support for the new Illustra video intelligence analytics on the Illustra Pro mini-dome IP cameras to automatically analyze captured video and alert users of specific motion detected activities through event linking.

The exacqVision VMS is accessed with the freely distributed exacqVision client software (Windows/Linux/Mac), the exacqVision free web browser client available for all leading web browsers (Google Chrome, Firefox, Internet Explorer, Safari and Opera), as well as the free Exacq mobile app for iOS, Android and Windows Phone 8 devices. The VMS software is included with pre-configured exacqVision NVR servers or it can be installed on third-party Windows or Linux-based systems.

For more information on this exacqVision software release and other new updates and offerings, go to www.exacq.com.

- End -

About Exacq
Exacq Technologies is part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Exacq Technologies (
www.exacq.com) designs and manufactures the cross-platform, open-architecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-platform (Windows/Linux/Mac) client, most web browsers and via the free Exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world via authorized resellers and distributors.

About Tyco Security Products
Tyco Security Products is the most comprehensive world-leading premium access control, video, and intrusion solutions provider in the security industry. Tyco Security Products conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.

Share On
Share