Tyco Security Products introduces mobile credentials with EntraPass 7.10

Share On
Share

Kantech’s flagship security software debuts the server-based EntraPass Go Pass credential app along with several key feature enhancements

WESTFORD, MA — December 7, 2016 – Tyco Security Products introduces the latest version of its EntraPass Security Software from Kantech with the new EntraPass Go Pass mobile application that allows card holders to use their mobile phones as an access control credential. EntraPass 7.10 software also includes updates to its Microsoft Windows Active Directory integration which now auto-synchronizes users, and extends the EntraPass Go Install app for installers to Android users.

Using the EntraPass Go Pass mobile app, cardholders can gain access to doors simply by pressing the appropriate icon of the door in the app, as they approach the door or from anywhere in the world. Using Wi-Fi or cellular connection, the app communicates directly with the access control system’s server, which allows organizations to leverage their existing card reader infrastructure and save on the cost of new card readers required with other mobile credentialing technologies.

“This newest release of EntraPass is focused on providing the ultimate in usability, giving our customers the efficiency and flexibility required in their day-to-day operations,” said Rajeev Dubey, Senior Product Manager, Tyco Security Products. “With EntraPass 7.10, both end users and installers benefit from greater functionality in mobile credentialing and one-touch configuration that enables significant costs savings on hardware and installation time.”

With the EntraPass Go Install mobile application, installers with Android devices can now configure KT-1 and KT-400 door controllers with one touch on a mobile device. Using a QR code scan that auto-fills the door controller's address and serial number, installation is faster and the potential for manual entry errors is eliminated. The app provides a wizard driven commissioning process that helps ensure that no device has been left un-commissioned. It also allows installers to store pictures and notes which will help with subsequent visits. The app further eases the install process with the ability to associate pre-configured Exacq-compatible cameras and DSC PowerSeries Neo devices. The newly added features in the app include the ability to edit relays and inputs, and view events.

The software allows for easy migration of legacy Kantech controllers to newer Kantech controllers without having to reprogram access levels, triggers, graphics, reports, or door exceptions. This allows installers to easily migrate a KT-200 or KT-300 into a KT-400 or a KT-100 into a KT-1.

EntraPass 7.10 now allows users to manage ASSA ABLOY Aperio wireless lock integrations through EntraPass Web client. EntraPass Go app now includes a redesign of quick actions of relays and inputs.

For more information, visit Kantech at www.kantech.com.

 

 

- End -

 

About Kantech
Kantech access control solutions from Tyco Security Products are now part of Johnson Controls, a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries.  Kantech access 
control technologies are ready to use right out of the box, and provide solutions that are compact, and easy to use for smaller businesses while scaling to meet the needs of larger businesses. Kantech solutions can easily link to American Dynamics video systems and DSC alarm panels to provide an integrated, holistic security solution. To learn more about Kantech products, visit www.kantech.com.

Tyco Security Products is now part of Johnson Controls, a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries. With its world-leading premium access control, video, location-based tracking and intrusion solutions, Tyco Security Products employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.

 

Share On
Share