Johnson Controls expands Illustra Flex camera line with 3MP compact mini-dome

Share On
Share

Flex Compact Mini Dome 3MPMILWAUKEE (October 24, 2017) – Johnson Controls introduces the Illustra Flex 3MP Compact Mini-Dome, a hard-working, outdoor quality day/night camera that can produce HD-quality images in low light conditions, and is small enough to fit seamlessly into discrete settings, whether it’s a retail store, bank, or healthcare facility.

Like other Illustra Flex cameras, the 3MP Compact Mini-Dome goes beyond H.264 and H.265 for bandwidth management via its powerful Illustra® IntelliZip compression technology that monitors and then adjusts system streaming parameters to match the level of activity in the camera’s field of view. IntelliZip also optimizes the bitrate when activity ceases to reduce network bandwidth and video storage needs.

Advanced VideoEdge® TrickleStor technology enables edge-based video recording, even in an outage. The camera will automatically detect interruptions between it and the NVR, record the video to its SD card, and seamlessly transfer video to the NVR’s hard drive for uninterrupted viewing once power is restored.

The factory-focused Flex 3MP Compact Mini-Dome is powered by Power over Ethernet (PoE) which reduces installation costs by eliminating the need for power cabling. Use of free Illustra Connect software makes configuration a quick and easy process. Installation time is further reduced through the use of remote firmware upgrades.

The Flex 3MP Compact Mini-Dome joins the rest of the Flex family in adhering to the rigorous standards of the Tyco Security Cyber Protection Program (CPP).

For more information on the Illustra Flex 3MP Compact Mini-Dome, visit www.illustracameras.com.

About Johnson Controls
Johnson Controls is a global diversified technology and multi industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.

###

 

CONTACTS:
Ryan Nolan
Global Public Relations Program Manager
Work + 1 414 524 6170
Mobile +1 414 378 9641
Ryan.P.Nolan@jci.com

Andrea Gural / Chelsie Woods
Eclipse Media Group on behalf of Johnson Controls
+1 207 233 7507 / +1 207 730 2396
agural@eclipsemediagroup.net / cwoods@eclipsemediagroup.net

Share On
Share