An Integrated Security Solution for Izmir Adnan Menderes Airport
Problem
Part of Turkey’s tourist region, Izmir is also a major import-export center. Because of burgeoning tourism and business needs, the area has seen a steady increase in air traffic, and Izmir Adnan Menderes Airport currently ranks fourth among the country’s airports for passenger traffic. The existing terminal was operating on a video surveillance and access control system originally installed in 2001. With the construction of a new domestic terminal, a platform needed to be put in place that would accommodate the use of existing technology at the old terminal, such as analog cameras, with a new, IP-based infrastructure and all the modern, attendant products in the new building.
Solution
The airport chose Tyco victor Unified security solution. Now using a single interface, security personnel gained the ability to manage live and recorded video via multiple VideoEdge NVRs. The VideoEdge NVRs allow the nearly 700 analog cameras located in the old terminal to migrate to the IP-based system, along with 600 new IP cameras that were installed in the new terminal. The airport’s new system also includes the Software House C•CURE 9000 access control platform for security and event management for monitoring activities, managing personnel and creating reports. The access control platform also serves as a redundant system to the victor security management system.
Products
American Dynamics
- victor Unified Management Software
- VideoEdge Network Video Recorders
Software House
- C•CURE 9000 Security and Event Management System