- Johnson Controls
- Customer Success Stories
- Stanford reduces peak energy demand by 17% and lowers GHG emissions by 68%
Stanford reduces peak energy demand by 17%
Stanford strengthens campus-wide energy performance through a transformational utility system redesign
Stanford University launched the Stanford Energy System Innovations (SESI) program to modernize its campus energy system to reduce fossil fuels, improve efficiency, and lower greenhouse gas emissions. As part of its long-term sustainability strategy, the university redesigned its central utility plant, transitioned to a heat-recovery-based hot water system, and connected 155 buildings through an optimized thermal network.
Impact Highlights
17% reduction in peak energy demand
Around $500,000 in annual cost savings
68% reduction in campus greenhouse gas emissions
Transforming an aging energy system to meet ambitious sustainability goals
Integrated solutions supported the SESI system redesign
To achieve Stanford’s energy performance goals, the university combined mechanical upgrades with advanced energy management solutions.
York OM heat recovery chillers formed the core of the new energy facility, capturing waste heat and supplying it through a campus hot-water network.
Thermal energy storage supported more efficient chilled and hot-water operations, and new electrical infrastructure enabled the transition away from the gas-fired trigeneration system.
OpenBlue Central Utility Plant Optimization helped operators evaluate real-time plant conditions, coordinate heat recovery, and optimize plant dispatch across the redesigned system.
These solutions supported SESI’s shift to a cleaner, more efficient, and more resilient energy model.
Upgrades across the campus produced measurable performance gains
The SESI upgrades resulted in several measurable efficiency improvements:
- 17% reduction in peak energy demand, driven by improved heat recovery and more efficient system-wide energy distribution
- 10% reduction in annual energy costs through lower electricity use and optimized plant operation
- 68% reduction in greenhouse gas emissions as a result of shifting away from combustion-based systems and increasing heat recovery
- Lower domestic water use enabled by the transition from a steam-based system to a more efficient hot-water network
- Improved heat recovery performance, allowing the central plant to make better use of thermal energy already being generated
- More stable and predictable system operation across the redesigned chilled-water and hot-water networks
These outcomes highlight how SESI’s integrated design continues to provide lasting environmental and operational benefits for the university.
About Stanford University
About the facility
- Stanford Energy Systems Innovations (SESI)
- Stanford, California, USA
- Central energy facility size: 125,614 sq ft
- Serves 155 buildings on campus
Solutions:
Similar stories
Georgia university achieves $90K in annual savings with data-driven maintenance
A leading university strengthened campus-wide performance by adopting data-driven maintenance. With clearer insights across 40 buildings, teams cut manual work and achieved nearly $90,000 in savings while supporting research productivity and student experience.
Hounslow Council Achieves 50% Carbon Emissions Reduction
Hounslow Council cut carbon emissions by 50% and saved 17M kWh through electrification and energy upgrades, advancing its 2030 net-zero goal.
Children’s of Alabama cuts natural gas use by 69% and strengthens mission-critical patient care
Children’s of Alabama is boosting efficiency and sustainability by partnering with Johnson Controls to link facilities to a central utility plant and upgrade systems, cutting energy use (including a 69% drop in natural gas) and operational costs while improving patient care.
Cortellucci Vaughan Hospital improves efficiency and sustainability with smart systems
Cortellucci Vaughan Hospital, Canada’s first smart hospital, uses OpenBlue and Metasys to reduce energy use, improve operational performance, and enhance patient experience, earning LEED Silver certification and ranking among top performers in energy efficiency.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)