- Johnson Controls
- Building Insights
- How OpenBlue turns sustainability into business value
4 examples that prove OpenBlue solutions aren’t just good for the planet – they’re good for business
Highlights
- OpenBlue digital solutions help organizations cut carbon emissions while boosting efficiency and lowering costs
- Connected data and digital optimization turn sustainability initiatives into measurable financial results
- Improving energy performance and modernizing infrastructure drives both emissions reduction and stronger business outcomes
Operating more sustainably is a worthwhile goal for any organization. In addition to reducing carbon emissions, it can also drive operational improvement and long-term business value. As organizations work to reduce their carbon footprint, improve efficiency and modernize infrastructure, facilities and real estate teams are also uncovering new opportunities to control costs and strengthen performance.
OpenBlue digital solutions are helping organizations accelerate these efforts by providing the insights and automation needed to advance sustainability goals and generate financial returns. Here are four examples – starting with Johnson Controls itself – that illustrate how that is possible.
1. Johnson Controls leads by example
Johnson Controls gave its own 2040 net zero commitment a boost by transforming one of its largest and most energy-intensive facilities: a 900,000-square-foot manufacturing, research and testing plant in Norman, Oklahoma.
The facility integrated the OpenBlue digital platform to manage and monitor a modernized central utility plant and an onsite solar-photovoltaic installation. OpenBlue supports the plant’s net zero goals by providing automated emissions reporting and deeper insights through operational data. The upgrades and implementation were achieved in a maximum production plant with minimal operational interruption.
The expected results demonstrate the direct link between digital optimization and financial performance:
- 43% reduction in greenhouse gas emissions
- Approximately $960,000 in annual energy savings
The Norman plant deployment of OpenBlue shows connected building data and optimization capabilities can support corporate sustainability commitments while delivering recurring cost savings. Most importantly, lessons learned through this project serve as a real-world decarbonization blueprint for global customers.
2. Stanford University transforms its energy system
As part of a program to modernize its campus energy system, Stanford University redesigned its central utility plant, transitioned to a heat-recovery-based hot water system and connected 155 buildings through an optimized thermal network. The new system required sophisticated coordination across electric heat recovery, thermal storage and water systems.
To help achieve their energy performance goals, the university complemented mechanical upgrades with advanced energy management solutions. OpenBlue Central Utility Plant Optimization empowered operators to evaluate real-time plant conditions, coordinate heat recovery and optimize plant dispatch across the redesigned system. Through data-driven insights and model-based control strategies, the system helps maintain stable campus conditions while adapting to changing loads and operational requirements.
The integrated design continues to provide lasting environmental and operational benefits for the university, including:
- 68% reduction in campus greenhouse gas emissions
- 15% reduction in domestic water use
- 17% reduction in peak energy demand
- 10% reduction in annual energy costs through lower electricity use and optimized plant operation
- Approximately $500,000 per year in savings compared to a modern plant baseline
Sustainability progress isn’t just about achieving large emissions reductions; it’s about building smarter, more efficient systems. Advanced digital energy optimization improves performance in complex environments and turns those operational efficiencies into quantifiable financial results.
See even more OpenBlue success stories
3. Standard Chartered Bank gains portfolio-wide visibility
For multinational institutions, the sustainability challenge often lies in scale. Managing hundreds of buildings across geographies makes identifying inefficiencies and prioritizing improvements significantly more complex.
Standard Chartered Bank implemented OpenBlue Net Zero Plus to gain enterprise-wide visibility across its Asia Pacific portfolio. The cloud-based solution integrates data from multiple systems to provide centralized visualization, analytics and performance benchmarking.
By leveraging real-time operational data, the organization was able to identify equipment faults, address inefficiencies and improve maintenance practices across hundreds of properties. The results are impressive:
- 13–15% improvement in operational efficiency
- 10–12% year-over-year energy reduction
- More than $600,000 in energy savings
- Visibility across 789 buildings and 1,760 connected assets across 10 countries
This example underscores the business case for portfolio-level digitalization. When energy and asset performance data are centralized and actionable, organizations can move from reactive maintenance to proactive optimization. This can help improve sustainability metrics and strengthen financial returns.
4. Children’s of Alabama cuts natural gas consumption – and costs
Sustainability initiatives must be carefully managed in healthcare settings to avoid compromising environmental conditions, reliability or security. When Children’s of Alabama expanded with a new acute care hospital, the organization required a solution that would enhance efficiency while ensuring uninterrupted support for critical clinical spaces.
The hospital implemented OpenBlue Central Utility Plant Optimization to digitally enhance plant performance. The solution enables real-time operational decision-making and continuous monitoring of the central utility plant serving five major campus buildings.
By improving visibility into plant operations and optimizing equipment performance, the hospital achieved:
- 69% reduction in natural gas use
- Approximately $681,000 per year in combined energy, operations and maintenance savings
For healthcare providers operating under tight budget constraints, this demonstrates that digital plant optimization can improve sustainability outcomes while preserving reliability and free up financial resources that can be redirected toward patient care.
Sustainability-minded digitalization as a business growth strategy
While these four examples come from very different sectors with distinct operational demands, several common themes emerge:
- Real-time performance visibility enables smarter operational decisions
- Advanced analytics and optimization reduce waste and inefficiency
- Portfolio-level data integration unlocks enterprise-wide improvements
- Sustainability gains translate directly into recurring cost savings
These results are documented outcomes – not hypothetical projections.
As regulatory pressures increase and corporate sustainability commitments become more ambitious, organizations need solutions that connect environmental responsibility with financial performance. OpenBlue digital solutions demonstrate that reducing emissions, improving energy efficiency and strengthening the bottom line are not competing goals. They mutually reinforce the outcomes of intelligent building management.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)