11 min read
May 26, 2026

Share

Highlights

  • Isolation rooms are designed to contain airborne infection, but that protection depends on consistent negative air pressure holding steady under real-world conditions
  • Even in a compliant room, airborne contaminants aren’t cleared instantly. At 12 air changes per hour, it still takes about 23 minutes to remove 99% of airborne particles from the space
  • While room specification is crucial to maintain pressure reliably, it must have coordinated airflow, responsive controls, and continuous visibility into performance

Isolation rooms serve a clear and essential role in hospitals: containing airborne infection. They’re used when patients may carry pathogens such as tuberculosis, measles, or other respiratory diseases that can stay suspended in the air and travel beyond the immediate bedside. These particles don’t simply fall to the ground, they can persist in the environment and can pose a serious risk over time.

Even in a well-designed isolation room, airborne contaminants aren’t removed instantly. At recommended ventilation rates, it can take more than 20 minutes to clear most particles from the air. During that period, the room must continue to contain what can’t yet be removed.

Maintaining containment during this period depends on negative pressure keeping airflow directed into the room rather than out of it, helping prevent airborne contaminants from escaping into adjacent spaces. In practice, maintaining that condition is challenging because isolation rooms are limited in number and heavily relied on. And they’re used not only for confirmed cases but often for suspected ones, under constant use and changing conditions driven by everyday clinical activity.

Under these everyday pressures, performance doesn’t always hold. A New York State research study observed inappropriate airflow in 38% of the isolation rooms tested; a stark reminder of how much progress is still needed.

Because airborne risk is invisible, these pressure failures aren’t always immediately apparent to the people relying on the room to perform. So, maintaining consistent air pressure is a continuous requirement that must hold under real operating conditions to keep risk contained within the isolation space.

See how Johnson Controls helps deliver consistent air pressure where it really matters — in your isolation rooms

Discover more

Why is maintaining consistency harder in practice?

Holding negative pressure in an isolation room is harder in practice than in design. The room has to maintain a defined pressure differential (typically at least –2.5 Pa), while keeping air moving in the intended direction under everyday hospital conditions.

Doors opening, HVAC loads shifting, and small leaks around ceilings, ducts or wall penetrations can affect room pressure. So, in a space that depends on directional airflow, even small changes can matter.

There’s also an operational cost to getting it wrong. After a patient leaves, a room could remain offline for 30 minutes to more than two hours while airborne particles are cleared. During periods of high demand, that limits availability given that even large hospitals typically have less than 10 isolation rooms.

Johnson Controls addresses this complexity by combining high-performance equipment with integrated, system-level control.

At the equipment level, creating this negative pressure starts with Johnson Controls YORK Solution Air Handling Units. They provide the backbone of airflow management. The units are engineered for precision and flexibility, with airflow capacities ranging from approximately 2,000 to 50,000 CFM for semi-custom units and up to 200,000+ CFM for fully custom applications. And this scalability allows hospitals to support anything from a single isolation room to an entire facility.

With reliability being an important factor, YORK units are factory-tested for low air leakage, helping ensure that designed airflow translates accurately into real-world performance.

Layered on top of the air-handling system, Johnson Controls Metasys building automation brings continuous monitoring and control to isolation environments. Metasys tracks room pressure in real time against defined setpoints and responds automatically by adjusting fan speeds and dampers as conditions shift. Stable room pressure is maintained through control of Venturi valves that react in less than one second, compensating for duct pressure changes and other system variations. Through the CE360 critical environment display, isolation room status is visible from nearby workstations using color coded indicators and halo lighting.

Real time automated monitoring is crucial for maintaining required negative pressure

Unfortunately, hospitals relying on intermittent manual verification methods could miss pressure reversals occurring between checks, leaving healthcare workers entering and exiting rooms without a reliable indication of containment status.

That’s why Johnson Controls designs isolation room systems, bringing air handling, filtration, and controls together under a single engineering approach. That shared design foundation allows the controls to interpret system behavior more accurately and respond more effectively as conditions shift. As a result, YORK and Metasys operate as an integrated system that delivers coordinated, adaptive pressure control with greater consistency during everyday operation.

Make isolation room performance something you can rely on

Isolation rooms are designed to contain risk, but in practice that depends on whether they can perform consistently under real conditions, not only at commissioning but throughout everyday use. When air pressure holds, containment holds. Patients, staff and adjacent spaces are protected, and a limited resource continues to operate as intended. When it doesn’t perform in this way, the impact extends beyond the room itself, affecting availability, confidence, and clinical workflow.

As a result, many hospitals are shifting their focus from room compliance to continuous performance, moving from verifying conditions at a point in time to maintaining them with visibility, control, and confidence built into the system. Johnson Controls supports this approach by bringing together airflow, sensing and control, helping isolation environments perform as intended in real world conditions.

See how Johnson Controls helps deliver consistent air pressure where it really matters — in your isolation rooms

Discover more

FAQs

1. How quickly are airborne contaminants removed from an isolation room?
Even in a properly designed room, contaminants aren’t removed instantly. At the recommended 12 air changes per hour, it can take approximately 20–25 minutes to remove 99% of airborne particles, making continuous containment during that time critical.

2. Why is maintaining consistent negative pressure challenging in real-world conditions?
Everyday hospital activities such as door openings, shifting HVAC loads, and small structural leaks can disrupt airflow. These dynamic conditions mean that maintaining stable pressure requires ongoing adjustment, not just initial design compliance.

3. How do air handling units (AHUs) support negative pressure in isolation rooms?
Air handling units create and maintain the airflow balance required for negative pressure by controlling the volume of air supplied to and exhausted from the room. By precisely managing this imbalance, AHUs ensure more air is removed than supplied, which keeps airflow moving into the room from adjacent spaces.

4. How can equipment such as Venturi valves maintain pressure stability?
Venturi valves regulate airflow instantly in response to pressure changes, often reacting in less than a second. This fast response helps maintain stable room pressure even during disruptions like door openings or system fluctuations, preventing loss of containment.

5. Why is real-time visualization important for isolation room performance?
Real-time displays, such as local indicators or dashboard systems, give staff immediate visibility into room status. This allows healthcare workers to quickly confirm whether the room is maintaining proper negative pressure before entering, supporting safer clinical decision-making.

Contact us

Please read our Privacy Notice for information on how we protect and manage your personal data. By completing this form and submitting your information, you confirm that you have reviewed, understood and accepted our privacy terms as well as our cookie terms.