Victoria Junior School Now Safe With Johnson Controls’ Fire Alarm System
Problem
Victoria Junior is an ethnically rich, medium-sized school in the town of Feltham, England. It serves around 300 pupils. A risk assessment was recently carried out at the school and the previous fire protection system was found to be inadequate. The school invited proposals to upgrade the system.
Solution
Victoria Junior School specified Tyco’s MZX addressable fire alarm system as the best value solution. The control panel selected for this project is part of the latest digital-based MZX Technology system family and offers greater functionality and advanced capacity in the number of field devices available on each loop, from 100 to 250, which makes for a more efficient and cost effective technology. Triple technology detection devices (which detect smoke, heat, and carbon monoxide gas) were installed at key risk points to provide a level of reassurance needed in a school where children’s safety is paramount.
Products
- MZX Technology System
- Triple Technology Detection Devices