Common Causes of Electrical Fires
Electrical fires are a Common Occurrence and, whilst not the most common type of workplace accident, can pose serious threats for commercial properties. They can be extremely dangerous, largely because under no circumstances can you throw water over them, meaning a Fire Extinguisher for Electrical Fires is usually required. Here’s how you can spot potential electrical risks, as well as some Fire Suppression advice.
How can an Electrical Fire start?
Five of the most common causes of electrical fires are:
1. Unsafe Wiring
In buildings that are several decades old, some of the electrical wiring might be outdated. If the amount of electricity used on site has increased over the years, for instance if more computers are now used in the workspace, then this can pose a safety risk. This is why it’s important to upgrade Building Controls and your Fire Detection System regularly.
2. Faulty Outlets
Worn out or faulty sockets are the main reason that properties need a fire extinguisher for electrical fires. Safety checks must be performed regularly on outlets, as their wiring can wear down over time.
3. High-Risk Appliances
Some electrical appliances can be considered high-risk when it comes to fire safety. Once again, these include old devices, including computers and kitchen appliances, as well as common domestic items such as electrical heaters.
4. Extension Leads
These increase the power demands on your electrical outlets. Thus, they pose a double risk by either breaking an old socket, or by causing an overload from adding too many devices to the extension lead. Where reasonable, it’s advised that appliances are plugged straight into an outlet, and you should never combine extension leads.
5. Lights
Light fixtures can create unseen electrical fire risks. Always check that you’ve installed bulbs that are within the recommended wattage limit, and never place flammable objects directly underneath lamps.
Fire Suppression & Safety Tips
Some basic fire safety tips that can limit risks from the above include:
- Install fire suppression systems such as a fire extinguisher for electrical fires
- Call an electrician to check your building’s wiring, especially of you’re unsure about its age
- Repair any loose sockets and replace faulty outlets
- Replace old appliances and inspect devices regularly for any faults
- Install more outlets to reduce dependence on extension leads
- If using extension leads, never run wiring under carpets and check their capacity
- Replace flickering lights and check that lamps and fixtures are positioned safely
- Ensure that you have modern Fire Alarms
Johnson Controls: Fire Extinguishers for Electrical Fires
We supply a wide range of Fire Extinguisher Solutions & Services that can be tailor-made to your business or property. To find out how we can help make your building safer, contact us today using the form on this page.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)