- Johnson Controls
- Media Center
- Kantech Entrapass 8.20 Product Update
Johnson Controls releases EntraPass v8.20 with seamless configuration and enhanced user functionality.
MILWAUKEE (January 14, 2020) – Johnson Controls is announcing the new EntraPass v8.20, which further simplifies how users remotely access the EntraPass go mobile app.
With EntraPass v8.20, EntraPass go Pass mobile app users gain improved search capabilities and other efficient upgrades to deliver remote and real-time access. EntraPass go Pass requests will no longer be attached to a selected SmartLink, eliminating the need to configure every connection. Users will now be able to access any inbound connection with little to no obstacles.
Enhanced users/card search functionality is also a significant enhancement of EntraPass v8.20. Users will be able to search for a profile, while keeping the search menu open – eliminating the need to start each search fresh. This solves the previous pain point of having to reopen the search menu, if a user had clicked on the wrong profile.
This update also opens the EntraPass Security Management Software to macOS users. EntraPass v8.0 will be compatible with the High Sierra system or higher.
Additionally, EntraPass v8.20 includes an ‘email’ field in the CSV report exports, which will be particularly beneficial for hattrix partners. This feature allows a manager to easily choose a set of accounts/owners and export email addresses, along with additional account statistics.
An additional benefit of EntraPass v.8.20 with EntraPass go Pass mobile app is the ability to view exacqVision video in hattrix, with seamless connection, easier configuration and no port forwarding. By enabling this feature within the server, the need for IT involvement is eliminated and customers will be able to connect their exacqVision NVR to the hattrix system.
For more information, visit www.kantech.com.
For more information:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com
Andrea Gural / Chelsie Woods
Eclipse Media Group on behalf of Johnson Controls
+1 207 233 7507
+1 207 730 2396
agural@eclipsemediagroup.net
cwoods@eclipsemediagroup.net

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)