- Johnson Controls
- Media Center
- Johnson Controls introduces LUX® KONOse for senior care market
Johnson Controls introduces LUX® KONOse for senior care market
First smart thermostat designed with the elderly in mind
The LUX® KONOse offers increased visibility, focused ease of use and adjustment assurance to create the best experience for residents of senior living facilities. The smart thermostat is the latest innovation from the Johnson Controls® brand of LUX Products, which are known for their intuitive design and technology.
MILWAUKEE – (April 23, 2020) – Johnson Controls today announced one of the first smart thermostat products to address the senior care market. Designed with seniors in mind, the LUX® KONOse offers increased visibility, focused ease of use and adjustment assurance to create the best experience for residents of senior living facilities. The Energy Star® certified thermostat is the latest innovation from the Johnson Controls brand of LUX Products, which are known for their intuitive design and technology. The introduction of the KONOse also marks the start of an exciting new collaboration between Johnson Controls and K4Connect, a leading technology partner for senior living communities.
“The KONOse enhances senior comfort through an easy-to-understand display and improved control for those with limited fine motor skills,” said Justin Pasquale, product management, thermostats and sensors at Johnson Controls. “It also provides connectivity, energy efficiency and cost savings for facility managers.”
The KONOse is an extension of the KONO smart suite of products for commercial facilities. To increase visibility, Johnson Controls designed the KONOse with larger primary and secondary digits as well as enhanced backlight options for ideal viewing in all environments.
“The KONOse enhances senior comfort through an easy-to-understand display and improved control for those with limited fine motor skills.”
— Justin Pasquale, product management, thermostats and sensors at Johnson Controls
When it comes to ease of use, large icons on the KONOse like a flame and snowflake call out heating and cooling functions, while an “emergency heat” function visible only to facility managers allows for passive monitoring. Users can rotate the thermostat’s dial to easily adjust the set temperature or push the dial to change HVAC modes. While adjusting the set temperature, the KONOse displays the new temperature as well as the current HVAC mode to ensure the user is setting the temperature in the right direction. These intuitive settings and tactile feedback are specifically tuned to users who have limited fine motor skills.
And on the connectivity front, the KONOse offers a host of features to help facility managers and residents alike effortlessly control comfort and savings. It leverages the power of the Z-wave smart home technology hub, allowing managers to easily connect all smart devices throughout the facility. The thermostat is also compatible with the LUX app so users can make temperature and scheduling adjusts from any device.
Through Johnson Controls design partnership with K4Connect, the LUX KONOse is now part of the most advanced enterprise technology solution in senior living. Built specifically for residents, staff and operators, K4Connect helps deliver a great experience for residents while providing insights to help operators improve their overall business health.
"Our K4Labs team tests hundreds of IoT devices for older adult-friendly design and functionality to ultimately determine the devices we prefer to integrate with,” said Derek Holt, executive vice president of development and chief operating officer at K4Connect. “It was exciting to work with Johnson Controls to design the KONOse and we look forward to bringing it to senior living communities across the nation."
The LUX KONOse is available now through K4Connect dealers. To learn more, visit pro.LUXProducts.com/KONOse.
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 105,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, York®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter
# # #
CONTACT:Jacquelyn Gozdowiak
Public Relations, BVK
Mobile + 1 414 232 8412
Jacquelyn.Gozdowiak@bvk.com
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)