Tyco Security Products introduces new all-in-one video recorder with integrated PoE+ camera ports

Share On
Share

exacqVision LC-Series Una Recorder simplifies installation and servicing

 

 exacqVision LC Series Una

WESTFORD, MA. March 22, 2016  — Tyco Security Products introduces the new exacqVision LC-Series Una all-in-one video recorder for faster, more efficient video security installation and service.

The exacqVision LC-Series Una recorder includes exacqVision video management system (VMS) software, server and integrated PoE+ camera ports. Users can connect up to 16 cameras per recorder and store up to 12 TB of video per system. The high output power supply provides up to 25 watts per camera and a maximum of 100 watts per 8 cameras and 200 watts per 16 cameras. Pre-loaded with exacqVision software for every IP camera port, Una recorders come with up to 16 exacqVision Start VMS software IP camera licenses. Users can view and administrate live and recorded video directly from the recorder using the included exacqVision client or remotely using a web browser or exacqVision client on a separate computer. The freely distributed client software can be installed on Windows, Linux or Mac systems.

Designed for easy installation, the LC-Series Una utilizes exacqVision EasyConnect to find, address and connect Illustra, Axis and Arecont Vision IP cameras to their network automatically and self-configure for motion-based recording. Therefore, users can easily plug in their IP cameras and start recording, significantly reducing installation time and labor. To further simplify maintenance, the LC-Series Una recorder enables users to remotely monitor and control power to individual cameras with no separate switch management software required.

“The new exacqVision Una recorder is the easiest IP video recorder to quote, install and service remotely managed power IP camera ports,” said Scott Dennison, Director of Marketing, Exacq Technologies. “The addition of this recorder product line gives our sales team a faster, more cost-effective way to support video security installations by remotely managing camera ports.”

The LC-Series Una is scalable with the entire line of exacqVision servers and software. Each LC-Series Una recorder includes a three-year hardware warranty and three years of free software updates.

For more information on this exacqVision recorder and other new offerings, go to www.exacq.com.

 

- End -

 

About Exacq

Exacq Technologies is part of the Security Products business unit of Tyco, the world’s largest pure-play fire protection and security company. Exacq Technologies (www.exacq.com) designs and manufactures the cross-platform, open-architecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-platform (Windows/Linux/Mac) client, most web browsers and via the free Exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world via authorized resellers and distributors.

About Tyco Security Products
Tyco Security Products and its leading brands conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential.  Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.

Share On
Share